ASLR seed in imx-optee

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ASLR seed in imx-optee

270 次查看
alexanderhoppus
Contributor I

Hi,

I'm looking in imx-optee and how ASLR seed is generated there. I see support for ELE https://github.com/nxp-imx/imx-optee-os/blob/lf-6.12.3_1.0.0/core/drivers/crypto/ele/ele.c#L610 , but there is no ele on my platform (imx8mp), however still the hardware rng is available in caam, but I don't see that it is used to seed ASLR, so system end up with seed 0 github.com/nxp-imx/imx-optee-os/blob/lf-6.12.3_1.0.0/core/arch/arm/kernel/boot.c#L112 what it seems is insecure.

0 项奖励
回复
3 回复数

224 次查看
alexanderhoppus
Contributor I

Hi @Harvey021 ,

thanks for your response, I don't think taking seed from dts will work, since seed need to be random and it should change on every boot, in other case aslr is unreliable. I don't think correct seeding will work with current codebase, I have several ideas how that can be resolved, but I'm not sure who is the right person / where is right place to discuss. Or maybe should I send MRs to optee/atf directly. But I would like first check if the ideas are feasible or not.

0 项奖励
回复

189 次查看
Harvey021
NXP TechSupport
NXP TechSupport

Hi @alexanderhoppus 

I've sent you system email.

 

Regards

Harvey

0 项奖励
回复

241 次查看
Harvey021
NXP TechSupport
NXP TechSupport

Hi, 

Have you tried to test what log or RNG past from FDT?

with unsigned long __weak get_aslr_seed(void) from boot.c

.....

offs =  fdt_path_offset(fdt, "/secure-chosen");
if (offs < 0) {
DMSG("Cannot find /secure-chosen");
goto err;
}
seed = fdt_getprop(fdt, offs, "kaslr-seed", &len);
if (!seed || len != sizeof(*seed)) {
DMSG("Cannot find valid kaslr-seed");
goto err;
}
 
return fdt64_to_cpu(fdt64_ld(seed));
 
err:
/* Try platform implementation */
return plat_get_aslr_seed();
 
Regards
Harvey
0 项奖励
回复