API

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

API

2,952件の閲覧回数
Bill_Bracken
Contributor I
I give.  Where is the "API" describing how to access the various peripherals of the MX53?
タグ(1)
0 件の賞賛
返信
3 返答(返信)

2,777件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

In order to access GPIO you can follow the kernel GPIO sysfs method that I posted here:

http://forums.freescale.com/t5/i-MX-Microprocessors/iMX28-SYSFS-and-GPIO/td-p/60938

 

For other peripherals I suggest to take a look at the Linux Reference manual that comes with the BSP documents.

 

Regards,

 

Fabio Estevam

0 件の賞賛
返信

2,777件の閲覧回数
Bill_Bracken
Contributor I

Daiane,

 

Thanks for responding.  The i.MX53 for example has GPIO (General Purpose I/O).  Does the Ubuntu developement environment provided by FreeScale have drivers, or an API, for the GPIO?  In general, you need functions to determine the direction of the I/O (input, output, tri-state), set the I/O, clear the I/O and get the current state of the I/O. Again, does FreeScale provide software to support the GPIO... as well as other peripherlas like CSPI, PWM ... etc.

 

bb

0 件の賞賛
返信

2,777件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee

I don´t understand your question. Can you, please, make yourself clearer?

 

Do you know unit_test?

0 件の賞賛
返信