ANDROID8.0 APP COLD BOOT

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ANDROID8.0 APP COLD BOOT

2,452件の閲覧回数
jeffery
Contributor III
Hi,friend
1.
I download the images from the android_O8.0.0_1.0.0_image_6dqpsabresd.tar.gz and android_N7.1.1_1.0.0_image_6dqpsabresd.tar.gz provided on the official website on the NXP development board MCIMX6Q-SDB.
After the system is running, use a simple hello world app (attached myapplication-debug.apk) to test the application cold start time.
 
 2.
The default display of the image is lvds 1024x768. The cold start conditions are as follows.
  Android 8.0 is shown below, which is about 1130ms
 Catch(12-26-10-4(12-31-08-57-30).jpg
   Android 7.1 is shown below, which is about 699ms
    CatchDF2D(12-26-(12-31-08-57-30).jpg
 3.
  Modify the system display to HDMI 1080p, the cold start situation is as follows
    Android 8.0 is shown below, which is about 1953ms
    Catch467C(12-26-(12-31-08-57-30).jpg
    Android 7.1 is shown below, which is about 932ms
    CatchB73C(12-26-(12-31-08-57-30).jpg
  4.
  Can our products based on Android8.0 imx6Q(HDMI interface and lvds interface) be at least similar to       Android7.1 or faster application cold start time?
 
 Thanks!
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,286件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi 贻才 林 

for fast boot one can try suggestions provided on

https://community.nxp.com/thread/448862 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,286件の閲覧回数
jeffery
Contributor III

I think they aren't my answer. they are about the optimize of system boot time.

My question is the optimize of application cold boot time. For example , when I open google maps or simple phone , it spent different time on Android7.1 and Android8.0.

Thanks!

0 件の賞賛
返信

2,286件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

for such kind optimizations suggest to try extended support with

Commercial Support and Engineering Services | NXP 

Best regards
igor

0 件の賞賛
返信