AN12195 Cortex-M4 build error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AN12195 Cortex-M4 build error

1,724 Views
Enuwai
Contributor III

A build error occurs because the following files are missing in the IAR project (audio_server.eww) in AN12195SW.zip.
where are these files?

fsl_shell.h
fsl_sai_sdma.c
fsl_sdma.c
fsl_shell.c

The SDK environment used is SDK_2.3.0_EVK-MIMX8MQ,
There are newer versions than this one, but they have more errors.

Labels (1)
0 Kudos
Reply
2 Replies

1,687 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Below files can be found in LPC family M4 SDK packages:
fsl_shell.c
fsl_shell.h
https://github.com/nxp-mcuxpresso/mcux-sdk/tree/main/devices/LPC54114/utilities

Below files can be found in i.MX8M Mini  SDK_EVK-MIMX8MM package:
fsl_sdma.c
fsl_sdma.h
fsl_sai_sdma.h
fsl_sai_sdma.c
M4 SDK can be found on link (build it for specific board):
https://mcuxpresso.nxp.com/en/welcome

Best regards,
Aldo.

0 Kudos
Reply

1,681 Views
Enuwai
Contributor III

Hi Aldo,

> Below files can be found in LPC family M4 SDK packages:
I have downloaded these files.

> Below files can be found in i.MX8M Mini SDK_EVK-MIMX8MM package:
If you use the files in SDK_2.13.0_EVK-MIMX8MM, a lot of build errors will occur.
I am using files from SDK_2.4.0_EVK-MIMX8MM.

Under this condition, a build error occurs (there are no files below)
  fsl_component_serial_manager.h
  fsl_memory.h
  fsl_component_generic_list.h

Best regards

0 Kudos
Reply