AMOLED 10.5" display with imx8m nano

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AMOLED 10.5" display with imx8m nano

3,159 Views
Rohan_R_E
Contributor II

Hello 

Hope you are doing well!

I have connected i.MX8M NANO EVK to the 10.5 inch AMOLED display and the display is not able to run the application which is running successfully when connected to monitor/desktop and there is this "failed to start terminate psplash-quit.service" error observed in the ssh terminal, attached image FYR. Please do guide me for what is this error coming and also steps to resolve the error. 

iMX8MNANO 

 

Labels (1)
0 Kudos
Reply
5 Replies

3,128 Views
arjunsuhasss
Contributor I

The "failed to start terminate psplash-quite service" error usually occurs when there is an issue with the graphical display service on the i.MX8M NANO EVK board Asphalt 9 mod apk....

0 Kudos
Reply

3,127 Views
Rohan_R_E
Contributor II
ok, then how can we fix this any idea/steps to be followed.
0 Kudos
Reply

3,134 Views
Rohan_R_E
Contributor II

The BSP version used:

Linux imx8mnevk 4.14.98-imx_4.14.98_2.1.0+g1a8a95a1ac05 #1 SMP PREEMPT Wed Jul 10 10:30:29 UTC 2019 aarch64 aarch64 aarch64 GNU/Linux

0 Kudos
Reply

3,139 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Which version BSP are you using?

0 Kudos
Reply

3,132 Views
Rohan_R_E
Contributor II
The BSP version used:

Linux imx8mnevk 4.14.98-imx_4.14.98_2.1.0+g1a8a95a1ac05 #1 SMP PREEMPT Wed Jul 10 10:30:29 UTC 2019 aarch64 aarch64 aarch64 GNU/Linux
0 Kudos
Reply