AI/ML Performance Data with GPU and NPU

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

AI/ML Performance Data with GPU and NPU

1,838 次查看
Jack-Cha
Contributor V

Hi 

The following illustration shows that both GPUs and NPUs support algorithms by NXP i.MX 8 series.
If you have AI/ML performance comparison data between GPU and NPU, please provide it.

A customer would like to know the performance compared btw GPU and NPU.

ArrowElectronics_0-1662463856586.png

Thanks.

Regards, 

James

 

标记 (1)
0 项奖励
回复
1 回复

1,833 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Arrow,

In case of Antutu V9 has a hard request on sampleRateShading feature(Vulkan 1.2 extension),  cannot run GPU test without this extension.

This is not well compatible with Khronos standard specification, which allow the extension feature absence by GPU vendor support.

https://www.khronos.org/registry/vulkan/specs/1.2-extensions/man/html/VkPhysicalDeviceFeatures.html

  • sampleRateShading specifies whether Sample Shading and multisample interpolation are supported. If this feature is not enabled, the sampleShadingEnable member of the VkPipelineMultisampleStateCreateInfo structure must be set to VK_FALSE and the minSampleShading member is ignored. This also specifies whether shader modules can declare the SampleRateShading capability.

In case of Android BSP release recommends Antutu V6 for 8MQ as V8 version requires huge memory.

For other benchmark I suggest to open a new case in our system due to nda document.

 

Regards

 

 

 

 

 

 

0 项奖励
回复