AHB write over flexSPI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

AHB write over flexSPI

2,197件の閲覧回数
jeff_hane
Contributor I

I'm looking at the linux driver for flexspi, fsl-flexspi.c and I'm working with an iMX8.   The reference manual states the following:  Memory mapped read/write access by AHB Bus.   However, the driver does memory mapped reads, it's still using the IP commands and TFDR register for writes.   

 Anyone know what this is the case?

thanks,

jeff

ラベル(2)
0 件の賞賛
返信
1 返信

2,046件の閲覧回数
art
NXP Employee
NXP Employee

The Linux FlexSPI driver for the i.MX8 processors still uses the IP commands for FlexSPI flash memory writes since this is more efficient and deterministic way of performing FlexSPI flash memory writes.


Have a great day,
Artur

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信