AHAB Application Programming Interface Reference Manual for the IMX8X

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AHAB Application Programming Interface Reference Manual for the IMX8X

33,236 Views
Gandalf-kern
Contributor IV

Do you have a specific link or download for the AHAB Application Programming Interface Reference Manual if one exists.  If not, then the HAB Version 4 Application Programming Interface Reference Manual and is there difference to be noted for AHAB?

Tags (2)
0 Kudos
Reply
1 Reply

33,231 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

 

The App note for the secure boot using AHAB for the i.MX8X is available at the following link: https://www.nxp.com/docs/en/application-note/AN12312.pdf

And you can refer to the security reference manual after request in the following link: https://www.nxp.com/webapp/sps/download/mod_download.jsp?colCode=IMX8QXPSRM&appType=moderatedWithout...

 

Hope it helps!

 

BR,

Ivan.

0 Kudos
Reply