AHAB Application Programming Interface Reference Manual for the IMX8X

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

AHAB Application Programming Interface Reference Manual for the IMX8X

32,396 次查看
Gandalf-kern
Contributor IV

Do you have a specific link or download for the AHAB Application Programming Interface Reference Manual if one exists.  If not, then the HAB Version 4 Application Programming Interface Reference Manual and is there difference to be noted for AHAB?

标记 (2)
0 项奖励
回复
1 回复

32,391 次查看
IvanRuiz
NXP Employee
NXP Employee

Hello,

 

The App note for the secure boot using AHAB for the i.MX8X is available at the following link: https://www.nxp.com/docs/en/application-note/AN12312.pdf

And you can refer to the security reference manual after request in the following link: https://www.nxp.com/webapp/sps/download/mod_download.jsp?colCode=IMX8QXPSRM&appType=moderatedWithout...

 

Hope it helps!

 

BR,

Ivan.

0 项奖励
回复