I am trying to use something like hsm_do_cipher or hsm_cipher_one_go to encrypt with AES 256 a small amount of data (32 bytes).
When I tried hsm_do_cipher I get an error that the handle is bad. If I use hsm_cipher_one_go I get a bad parameter error.
I tried to use this code to create my test:
https://github.com/nxp-imx/imx-secure-enclave/blob/1130c8bb820881ad037ba3f060e7fa70635fae3c/test/hsm...
I get this error from hsm_cipher_one_go:
SAB Error: SAB CMD [0x62] Resp [0x429] - MU sanity check failed / Invalid parameters.
aesencrypt: aesencrypt.c:164: hsm_do_cipher failed, err=0x4
Is there a way to determine what is wrong with my parameters? I see no errors when I create my key in a separate program. Files are created under /etc/ele.
Here is my code setting up the cipher_args:
memset(&cipher_args,0,sizeof cipher_args);
cipher_args.key_identifier = KEYID;
cipher_args.iv = SM2_IDENTIFIER;
cipher_args.iv_size = sizeof(SM2_IDENTIFIER);
cipher_args.flags = HSM_CIPHER_ONE_GO_FLAGS_ENCRYPT;
cipher_args.cipher_algo = HSM_CIPHER_ONE_GO_ALGO_ECB;
cipher_args.input = sp;
cipher_args.input_size = slength;
cipher_args.output = od;
cipher_args.output_size = slength;Solved! Go to Solution.