AAOS - Run software on M4

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

AAOS - Run software on M4

ソリューションへジャンプ
2,247件の閲覧回数
Danilo3
Contributor III

Hello everybody,

I'm currently using AAOS version 13.1.0_1.1.0 on my i.MX 8QuadMax MEK.

I have modified the SCFW in order to have FlexCAN in the list of pads in M4 1 partition.

If I have an application, let's say "M4_1_image.bin", how can I make it run on the M4 processor?

Which are the steps to somehow include such bin into the ${MY_ANDROID}/out/target/product/mek_8q directory, then flash it to the board?

Thank you for your support.

ラベル(1)
0 件の賞賛
返信
1 解決策
2,200件の閲覧回数
Danilo3
Contributor III

Hello,

I managed to understand where to place my executable. For M4 core 1, it has to replace file imx8qm_m4_1_default.bin in the directory ${MY_ANDROID}/vendor/nxp/fsl-proprietary/mcu-sdk/imx8q/ (keeping the same name as the default one).

Then I just rebuilt the bootloader and flashed the image to the board.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,219件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

 

You can download the Quickstar guide that show you how to boot and start with Cortex M4 on android.

https://www.nxp.com/docs/en/quick-reference-guide/ANDROID_QUICK_START_GUIDE.pdf

 

Regards

0 件の賞賛
返信
2,201件の閲覧回数
Danilo3
Contributor III

Hello,

I managed to understand where to place my executable. For M4 core 1, it has to replace file imx8qm_m4_1_default.bin in the directory ${MY_ANDROID}/vendor/nxp/fsl-proprietary/mcu-sdk/imx8q/ (keeping the same name as the default one).

Then I just rebuilt the bootloader and flashed the image to the board.

0 件の賞賛
返信