A part of i.MX7S eFuse could not be read.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

A part of i.MX7S eFuse could not be read.

ソリューションへジャンプ
1,172件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

Our customer tried reading a i.MX7S efuse, and succeeded reading lot number programmed in 0x410[31:0] and 0x420[10:0].
However, 0x420[31:11] was all "0".
According to Table 6-19 of IMX7DRM Rev.0.1, wafer number and X/Y coordinate should be programmed in the field.
They executed the process chapter 6.4.3.1.1 and 6.4.3.1.2, so we think the procedure was not wrong since they could read 0x410[31:0] and 0x420[10:0] correct.
Do think think why 0x420[31:11] cannot be read?

Best Regards,
Satoshi Shimoda

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 解決策
1,039件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi 

customer should use unique ID is a full 64bit value, even 0x420[31:11] was all "0" and

it is correct unique value. That was confirmed by app team (please create service request

for additional details). Additonal info provided: NXP does not provide the actual decoding to customers.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,040件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi 

customer should use unique ID is a full 64bit value, even 0x420[31:11] was all "0" and

it is correct unique value. That was confirmed by app team (please create service request

for additional details). Additonal info provided: NXP does not provide the actual decoding to customers.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信