A number of max users of i.MX6 Android BSP.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

A number of max users of i.MX6 Android BSP.

ソリューションへジャンプ
1,198件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

We have a question about i.MX6 Android BSP (kk4.4.2_1.0.0-ga).

You know, a number of the max users (config_multiuserMaximumUsers) is set to "8" in this BSP.

Would you let me know the reason why it is set to "8"?

Best Regards,

Satoshi Shimoda

ラベル(5)
0 件の賞賛
返信
1 解決策
1,091件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

seems this is default value provided by Android sources, as it is

most commonly used

[MOD] Add multi-user support to Android 4.2 … | Android Development and Hacking | XDA Forums

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,092件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

seems this is default value provided by Android sources, as it is

most commonly used

[MOD] Add multi-user support to Android 4.2 … | Android Development and Hacking | XDA Forums

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信