A number of max users of i.MX6 Android BSP.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

A number of max users of i.MX6 Android BSP.

Jump to solution
1,151 Views
satoshishimoda
Senior Contributor I

Hi community,

We have a question about i.MX6 Android BSP (kk4.4.2_1.0.0-ga).

You know, a number of the max users (config_multiuserMaximumUsers) is set to "8" in this BSP.

Would you let me know the reason why it is set to "8"?

Best Regards,

Satoshi Shimoda

Labels (5)
0 Kudos
Reply
1 Solution
1,044 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

seems this is default value provided by Android sources, as it is

most commonly used

[MOD] Add multi-user support to Android 4.2 … | Android Development and Hacking | XDA Forums

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,045 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

seems this is default value provided by Android sources, as it is

most commonly used

[MOD] Add multi-user support to Android 4.2 … | Android Development and Hacking | XDA Forums

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply