A Quick Boot OS for the Quick Start Board?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

A Quick Boot OS for the Quick Start Board?

3,306件の閲覧回数
Geoff1z
Contributor I
I'm interested to know if anyone is working on a port or eCos (or other fast boot OS) for the i.mx53 QSB.  Linux just doesn't meet our requirements, I'd be happy to be proven otherwise but it seems the best we could hope for on a tuned linux implementation would be about 700ms.
ラベル(1)
0 件の賞賛
返信
6 返答(返信)

3,221件の閲覧回数
Geoff1z
Contributor I
0 件の賞賛
返信

3,221件の閲覧回数
XXiao1z
Contributor III
this is less imx535 related, we can discuss this offline i think
0 件の賞賛
返信

3,221件の閲覧回数
Geoff1z
Contributor I

We wish to capture images in about 200 - 300 ms from power up (i.e. power applied, not from sleep, from a true cold start).

 

It appears from various discussions I've had that linux cannot be coerced to boot faster than about 700ms. So that leaves:

  1. do something tricky while booting linux 
  2. boot a different OS (like eCos) that doesn't have linux's limitations
  3. boot no OS and run bare metal

Hope this makes sense.

0 件の賞賛
返信

3,221件の閲覧回数
XXiao1z
Contributor III
while capture images in real time is quite normal, but i don't see why it requires a 700ms boot up time?
0 件の賞賛
返信

3,221件の閲覧回数
Geoff1z
Contributor I

We need to capture images from a cmos sensor preferably through the h.264 encoder to memory.

If necessary we could capture the images raw to memory and pass them through the encoder later (not preferred but possibly the only way).

Achieving the fast boot with linux would be a good answer as its not clear how we might access the hardware encoder from a different OS since they seem to be only supported via linux drivers.  i.e. eCos has the boot speeds but integrating in support for the hardware encoder may be a headache.

0 件の賞賛
返信

3,221件の閲覧回数
XXiao1z
Contributor III

what service do you need immediately after the boot up? network? storage? video on screen?

while 700ms is challenging if you don't need much right at the bootup moment it's still possible.

0 件の賞賛
返信