A Question about ANATOP Reg Offset.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

A Question about ANATOP Reg Offset.

Jump to solution
2,896 Views
simmisxu
Contributor III

Hi,

     In RM, ANATOP register offset is described like:

anatop.PNG
      How do I understand the offset (4d * i) ?

Thanks,

Simmis

Labels (1)
1 Solution
2,688 Views
simmisxu
Contributor III

d means decimal. This is a stupid question. Sorry!

View solution in original post

0 Kudos
Reply
3 Replies
2,688 Views
Yuri
NXP Employee
NXP Employee

You may use headers from the Platform SDK, in particular

sdk\include\mx6dq\registers\regsccmanalog.h


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,688 Views
simmisxu
Contributor III

Thanks, Yuri! I also noticed the regspmu.h. Very helpful!

0 Kudos
Reply
2,689 Views
simmisxu
Contributor III

d means decimal. This is a stupid question. Sorry!

0 Kudos
Reply