Hi @jakub_zigacek Could you provide me with DDR 4GB patch file? The file is such like this
8MP2GB_BSP_1.4.1_ver_01.zip.
I can install Win10 with DDR 2GB. Because there is a compatibility issue between sdcard and 8MP. So I changed others sdcard, and my device can install Win10 normally and apply the 2GB patch file you provided.
But the same device has DDR 4GB. The hardware is the same, except that the DDR has changed from 2G to 4G.
When the device with 4G DDR, enter winpe and prepare to install win10. When progress start to 1%. the system display BSOD.
The message shows STSTEM THREAD EXCEPTION NOT HANDLED. I think this is 4G DDR parameters setting issue.
So, Could you provide me 4G DDR patch files, such like 2GB patch files?
The DDR is MT53E1G32D2FW-046 WT:B