8M Mini PCIe Clock Generation Termination

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

8M Mini PCIe Clock Generation Termination

ソリューションへジャンプ
4,786件の閲覧回数
adevries
Contributor V

Hello,

If I want to use the 8M Mini to generate my PCIe clock signal, does that signal need any external terminating resistors? Or does it have internal 50 ohm terminations?

Thanks

ラベル(1)
0 件の賞賛
返信
1 解決策
4,658件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi adevries

 

corrected:

it is configurable using bit 3 register CMN_REG064
described in sect.11.4.3.1.102 (CMN_REG064)

i.MX 8M Mini Applications Processor Reference Manual

 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
4,659件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi adevries

 

corrected:

it is configurable using bit 3 register CMN_REG064
described in sect.11.4.3.1.102 (CMN_REG064)

i.MX 8M Mini Applications Processor Reference Manual

 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

4,575件の閲覧回数
marcelziswiler
Senior Contributor I

I really don't think this is true. We added external termination but now the amplitude of the clock is way too low. Removing those external 50 ohm termination resistors again improves the situation but it looks like further tweaking of undocumented registers from the DWC IP is required. Could you please reveal details about how/what exactly one may set to increase the clock swing? Thanks!

0 件の賞賛
返信