8-bit eMMC interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

8-bit eMMC interface

3,836 Views
shwethanarayan
Contributor I

Hi NXP team,

 

We are using i.MX 6 processor MCIMX6G3CVM05AB for one of our project.

Can we connect this 8-bit eMMC to ushdc-2(SD2 ) interface. We are using this eMMC as the primary booting option.

Also can we use UUU to flash the eMMC? What changes need to be done?

Please let me know your feedback.

 

Regards

Shwetha

0 Kudos
Reply
4 Replies

3,811 Views
shwethanarayan
Contributor I

Hi Team,

 

Can anybody answer me on this query.

We are using i.MX 6 processor MCIMX6G3CVM05AB for one of our project.

Can we connect this 8-bit eMMC to ushdc-2(SD2 ) interface. We are using this eMMC as the primary booting option.

Also can we use UUU to flash the eMMC? What changes need to be done?

Please let me know your feedback.

 

Regards

Shwetha

0 Kudos
Reply

3,831 Views
joanxie
NXP TechSupport
NXP TechSupport

refer to the Table 5-6. MMC/eMMC Boot Fusemap of imx6ul reference manual, BOOT_CFG2[5-7] can choose bus width:

Bus Width:
000 - 1-bit
001 - 4-bit
010 - 8-bit
101 - 4-bit
DDR (MMC 4.4)
110 - 8-bit
DDR (MMC 4.4)
Else - Reserved

 

then try the patch to support 8bit emmc

diff --git a/include/configs/mx6ul_14x14_evk.h b/include/configs/mx6ul_14x14_evk.h

index aabe2f7..b05b71f 100644

--- a/include/configs/mx6ul_14x14_evk.h

+++ b/include/configs/mx6ul_14x14_evk.h

@@ -426,4 +426,6 @@

#include "mx6ul_14x14_evk_android.h"

#endif

 

+#define CONFIG_MX6UL_EVK_EMMC_REWORK

+

#endif

 

 

 

0 Kudos
Reply

3,825 Views
shwethanarayan
Contributor I

Hi NXP Team,

 

Thanks for the reply.

Our custom board has iMX 6 processor  MCIMX6G3CVM05AB.

Please answer my below questions with YES or NO.

1. Can we connect this 8-bit eMMC to ushdc-2(SD2 ) interface?

2.Also can we use UUU to flash the eMMC mentioned in question 1?

 

Regards

Shwetha

0 Kudos
Reply

3,807 Views
joanxie
NXP TechSupport
NXP TechSupport

did you see my patch? this is for how to support 8bit emmc the answer is yes of course

0 Kudos
Reply