6ull ddr3 configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

6ull ddr3 configuration

1,232件の閲覧回数
lvjz
Contributor I

Hi, we used nxp 6ull and winbond ddr3(w631GG6mb).The system occasionally crashes .We did not encounter this problem when using Samsung ddr3. Winbond engineers are helping to solve this problem.
When Winbond engineers deal with the problem,he need a memory configuration so that the memory clock keeps output.We have tried 21B_0004H [15:8] set to 0 ,and 21B_0404H [0] set to 1. But the memory clock still has a break.How do I set registers to keep the memory clock uninterrupted?

ddrclk.png

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,131件の閲覧回数
lvjz
Contributor I

We have used the script to configurate the DDR3 . I’d like to know which register and how to config  so that   I can keep the DDR3 clock uninterrupted. We tried disable  MAPSR[PSD], MDPDC[PWDT_1], MDPDC[PWDT_0], MDPDC[PRCT_0],MDPDC[PRCT_1]. ,but these don't work .

0 件の賞賛
返信

1,131件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

About the DDR configuration you can use the script https://community.nxp.com/docs/DOC-333791 

0 件の賞賛
返信