5-inch circular touch LCD display interfacing with imx8qxp

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

5-inch circular touch LCD display interfacing with imx8qxp

1,870件の閲覧回数
vsuneja63
Contributor III

Hi,

Thanks!

I am planning to interface a 5-inch circular touch based LCD display with imx8qxp-mek on android using LVDS to HDMI interface. Does imx8qxp support 3rd party touch screen display or any other configurations need to be modified to include the support?

Does the android HMI will be adjusted here itself on circular display. Looking forward for your response asap.

Regards,

Vipul Kumar

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,838件の閲覧回数
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @vsuneja63,

I hope you are doing well.
Please accept my apologies for the delay in response.
 
i.MX8QXP can support circular displays.
 
One can refer to i.MX 8X to look for various display interface support in imx8qxp.
 
Thanks & Regards,
Sanket Parekh
0 件の賞賛
返信

1,833件の閲覧回数
vsuneja63
Contributor III

Hi Sanket,

Thanks for your response!

Can you please provide any reference for 5 inch circular LCD touch display compatible with imx8qxp? I could find a few but doesn't seems to be authentic. Any suggestion on this will be very helpful.

Regards,

Vipul Kumar  

0 件の賞賛
返信

1,806件の閲覧回数
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @vsuneja63 

I hope you are doing well.

i.MX8QXP supports the below-mentioned display interfaces.
Screenshot from 2023-03-13 16-06-39.png
One can use any circular display that has support for the above-mentioned display interfaces.
 
Thanks & Regards,
Sanket Parekh

0 件の賞賛
返信