5-inch circular touch LCD display interfacing with imx8qxp

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

5-inch circular touch LCD display interfacing with imx8qxp

1,825 Views
vsuneja63
Contributor III

Hi,

Thanks!

I am planning to interface a 5-inch circular touch based LCD display with imx8qxp-mek on android using LVDS to HDMI interface. Does imx8qxp support 3rd party touch screen display or any other configurations need to be modified to include the support?

Does the android HMI will be adjusted here itself on circular display. Looking forward for your response asap.

Regards,

Vipul Kumar

0 Kudos
Reply
3 Replies

1,793 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @vsuneja63,

I hope you are doing well.
Please accept my apologies for the delay in response.
 
i.MX8QXP can support circular displays.
 
One can refer to i.MX 8X to look for various display interface support in imx8qxp.
 
Thanks & Regards,
Sanket Parekh
0 Kudos
Reply

1,788 Views
vsuneja63
Contributor III

Hi Sanket,

Thanks for your response!

Can you please provide any reference for 5 inch circular LCD touch display compatible with imx8qxp? I could find a few but doesn't seems to be authentic. Any suggestion on this will be very helpful.

Regards,

Vipul Kumar  

0 Kudos
Reply

1,761 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @vsuneja63 

I hope you are doing well.

i.MX8QXP supports the below-mentioned display interfaces.
Screenshot from 2023-03-13 16-06-39.png
One can use any circular display that has support for the above-mentioned display interfaces.
 
Thanks & Regards,
Sanket Parekh

0 Kudos
Reply