Hi NXP Team
In NXP web side, we try the 5.10.52_2.1.0 Demo Image can not boot up on imx8mq evk Demo board.
Do you have any advice?
The log message will be show " Preparing Automatic Repair Loading files..." in Debug message.
Solved! Go to Solution.
Hi NXP Team
The Question can closed.
We know why can not boot.
Thanks NXP.
Which version of the i.MX8MQ board are you using? And could you tell us are you download images to emmc or SD card? Have you finished download?
Hi NXP Team
The IMX8M EVK Demo board.
I can fine the (170-39920 REV A) (TR19210881) (2018 NXP) in IMX8M EVK Demo board.
Download image to SD card.
Yes I already finished download. (I try many time).
How about the boot command line setting when u-boot boot up. I will try it on my board and then tell you the result.
Hi NXP Team
I used the demo image and flash to SD card.
Then I try to boot form SD in Demo board.
Uboot command :
#env default -a
#save
Hi NXP Team
I try the 5.10.72 demo Image , the result is the same with 5.10.52.
When the debug port show " Booting /efi\boot\bootaa64.efi"
Then system will be show " Preparing Automatic Repair"
"Loading files...."
Then system hung up.
Hi NXP Team
The Question can closed.
We know why can not boot.
Thanks NXP.
Did the u-boot boot up?
Hi NXP
Yes, it's already boot up u-boot.
Do you have the imx8mq evk demo board? You can try it, then you will be know it.