Hi,
I will use the 4Gx8bits hynix nand on my own board.
I have to upgrade this nand flash on imx50_RD3 evk. I tried to upgrade the hynix nand with mfg tool, and it succeded from the log, but I found that the written data to nand is different from original data when readback. there are 13 bytes unexpected after every 512 bytes from readback data.
I can write the nand flash correctly when I used the nand write cmd to write the nand in uboot.
is this relatd to mtd-utils (nandwrite, the version not support 4Gx8bits nand?) ?
do they need to modify the nand_device_info.c ?
please help,thanks a lot
h27ubg8t2atr.pdf