4098x2560 resolution lcd support by i.MX 8MQ' HDMI

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

4098x2560 resolution lcd support by i.MX 8MQ' HDMI

跳至解决方案
2,489 次查看
Jack-Cha
Contributor V

Hi i.MX Champs.

A customer is trying to interface a 4098x2560 resolution LCD using the HDMI port of the iMX 8qm which is able to support upto 4096x2160@60Hz via HDMI 2.0a.

I would like to ask you if i.MX 8MQ can support 4098x2560 LCD via HDMI regardless of framerate. 

Also, please let me know if there is an NXP processor that supports 8K display.

Thanks. 

Regards, 

James

 

 

0 项奖励
回复
1 解答
2,458 次查看
JorgeCas
NXP TechSupport
NXP TechSupport

Hello, here Jorge.

The maximum output resolution trough HDMI of the i.MX8MQ it is up to 4096x2160@60Hz.

I checked the display and the resolution it is more than the supported by the i.MX8MQ, I saw the part number on internet, and it comes with a HDMI adapter, please check if that adapter can rescale the 4K resolution from the i.MX8MQ to the 4098x2560 resolution of the DBT066MONO.

Best regards.

在原帖中查看解决方案

4 回复数
2,464 次查看
Jack-Cha
Contributor V

Hi Jorge

Can you please check if the monochrome LCD with 4098x2560 resolution can be applicable with i.MX 8 MQ?

This is asked since the monochrome LCD does require less memory support. 

Here is attachment of LCD DATASHEET what they slected.  

Regards, 

Jack

0 项奖励
回复
2,459 次查看
JorgeCas
NXP TechSupport
NXP TechSupport

Hello, here Jorge.

The maximum output resolution trough HDMI of the i.MX8MQ it is up to 4096x2160@60Hz.

I checked the display and the resolution it is more than the supported by the i.MX8MQ, I saw the part number on internet, and it comes with a HDMI adapter, please check if that adapter can rescale the 4K resolution from the i.MX8MQ to the 4098x2560 resolution of the DBT066MONO.

Best regards.

2,446 次查看
Jack-Cha
Contributor V
Hi Jorge
Customer checked the LCD is able to support 4K by rescaling. They will use i.MX 8MQ for their 3D printer project.
Thanks.
2,473 次查看
JorgeCas
NXP TechSupport
NXP TechSupport

Hello, here Jorge.

Thank you for contact support team.

The maximum output resolution trough HDMI of the i.MX8MQ it is up to 4096x2160@60Hz.

Right now, we do not have any processors for 8K solutions.

Best regards.

0 项奖励
回复