4 Camera input, vpu encode and image processing, is i.mx53 capable?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

4 Camera input, vpu encode and image processing, is i.mx53 capable?

3,005 Views
YuLin
Contributor I

I am searching a hardware solution for the follow requirement:

1. 4 camera input, resolution 640*480. NTSC or PAL

2. The above 4 camera input will be encode with VPU h264 into SD Card.

3. At the same time, these 4 frames will be processed by a simpel image function.

 

According to reference for i.mx53, it can process up to 4 encode/decode work simultaneously.

 

i.mx53 can afford to this work, is it right?

Tags (1)
0 Kudos
Reply
4 Replies

2,718 Views
JasonShi1z
Contributor I

We have question like yours too, but our usb cameras are H.264, not raw data, so we want to connect 8 cameras to iMX53, and use iMX53 to decode h264 stream at same time. Each camera is QVGA resolution.
I also want to know that i.MX53 can handle the task or not.

0 Kudos
Reply

2,718 Views
daiane_angolini
NXP Employee
NXP Employee

VPU is the "block" which encode and decode video, like taking YUV and giving H264.

 

By default, imx53 BSP has one "special" camera input (csi). The camera input is done by some hardware specific (please, take a look on IPU documentation for details).

 

As I know, there is only CSI0 and CSI1, in other words, there is only 2 "hardware camera inputs".

 

In case you´re using 4 USB, I don´t know if USB bus will be fast enough for all video instances.

 

But wait. There are cameras that gives H264, is it your case?

0 Kudos
Reply

2,718 Views
YuLin
Contributor I


Daiane Angolini said:

4 encode/decode instance is not the same as 4 camera inputs.

 

* I can understand it.

 

I don´t believe imx53 has more than 2 camera input. Well, you can use 4 USB cameras...

* Now I am trying 4 USB camera.

 

Thank you.

0 Kudos
Reply

2,718 Views
daiane_angolini
NXP Employee
NXP Employee

4 encode/decode instance is not the same as 4 camera inputs.

 

I don´t believe imx53 has more than 2 camera input. Well, you can use 4 USB cameras...

0 Kudos
Reply