4-5 second video lag while live streaming data through a wifi borescope in sabresd

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

4-5 second video lag while live streaming data through a wifi borescope in sabresd

1,347件の閲覧回数
himanshugusain
Contributor III

Hi

I have few sabresd boards from freescale which runs on Android 4.4 & 5.0.2  

Recently I integrated the Wi-Fi Streaming application in all the tools

& found their is a lag of 4-5 in the data received in the Tool when connected to a borescope.

What could be possible issue , Is it something to do with the VPU in imx6 side

Regards

Himanshu

ラベル(4)
0 件の賞賛
返信
2 返答(返信)

1,206件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Himanshu

had you tried to measure delays without wi-fi,

for vpu one can try to enable low-latency plugin as described in

RTSP gstreamer and vpudec 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,206件の閲覧回数
himanshugusain
Contributor III

Igor

What do you mean by measure delay without wi-fi

You want me to store media file locally in tool & play from there

& compare that with a good known device.

Regards

Himanshu

0 件の賞賛
返信