4.14.78 fetch error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,539件の閲覧回数
coindu
Contributor IV

   Hi ALL:

         a):mkdir imx-yocto-bsp 

         b):cd imx-yocto-bsp

         c): repo init -u https://source.codeaurora.org/external/imx/imx-manifest  -b imx-linux-sumo -m imx-4.14.78-1.0.0_ga.xml 

         d):repo syn

 

         Fetching projects: 88% (8/9)
fatal: Couldn't find remote ref refs/heads/rocko-4.14.62-1.1.0_beta
error: Cannot fetch meta-fsl-bsp-release from https://source.codeaurora.org/external/imx/meta-fsl-bsp-release

       rocko-4.14.62-1.1.0_beta is not exist  .it should be replace sumo-4.14.62-1.0.0_beta or  sumo-4.14.78-1.0.0_ga ?

ラベル(1)
0 件の賞賛
返信
1 解決策
2,134件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

I use the same command as yours, and repo sync the 4.14.78 successfully without errors., it seems that your network connection issue, could you open https://source.codeaurora.org/external/imx/meta-fsl-bsp-release on the linux environment? try to delete imx-yocto-bsp and bin folder, then build again accroding to i.MX Yocto Project User's Guide of 4.14.78 version

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,135件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

I use the same command as yours, and repo sync the 4.14.78 successfully without errors., it seems that your network connection issue, could you open https://source.codeaurora.org/external/imx/meta-fsl-bsp-release on the linux environment? try to delete imx-yocto-bsp and bin folder, then build again accroding to i.MX Yocto Project User's Guide of 4.14.78 version

0 件の賞賛
返信