30Mbit/s clocked serial interface

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

30Mbit/s clocked serial interface

1,069 次查看
frankambrosius
Contributor II

Hi All,

I have a proprietary data connection to/from a data acquisition system that produces a NRZ encoded serial data stream of max 30Mbit/s. The connection shall be bi-directional.

What interface can be best used to receive this data in the iMX6? Would SPI be an option? Or are there better options?

Thank you in advance for your suggestions!

标签 (1)
标记 (2)
0 项奖励
回复
1 回复

923 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi Frank,

You could take a look at the application note AN3020 “Configuring and Using the SPI”:

http://www.nxp.com/assets/documents/data/en/application-notes/AN3020.pdf

Regarding the specific information of the i.MX6 processor, you could refer to Table 51 “ECSPI Master Mode Timing Parameters” of i.MX 6Dual/6Quad Datasheet:

http://www.nxp.com/assets/documents/data/en/data-sheets/IMX6DQCEC.pdf

 
Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复