#2 NAND Flash Boot Flow and Boot Control Blocks.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

#2 NAND Flash Boot Flow and Boot Control Blocks.

1,169 Views
takashitakahash
Contributor III

Dear community.

i.MX6DQ RM of sect 8.5.2.2 NAND Flash Boot Flow and Boot Control Blocks (BCB) description.

Driver reads raw 2112 bytes of first sector and runs through software ECC engine that determines whether FCB data is valid or not.

In Figure 8-5. FCB Search Flow, it has become Read 4K, and ReadCount ++.

Would you please more detail information.

Labels (2)
0 Kudos
Reply
1 Reply

1,059 Views
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

for searching FCB data iROM reads raw 2112 bytes.

Except RM there is no more detailed information, sorry.


Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------