12-bit Bayer RGB format CMos sensor support on i.MX6Q

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

12-bit Bayer RGB format CMos sensor support on i.MX6Q

ソリューションへジャンプ
4,752件の閲覧回数
FeiShen
NXP Employee
NXP Employee

   Does anyone know how to run 12-bit Bayer RGB format CMos Sensor on i.MX6Q?

   Is the HW connecting method to connect 12-bit data to i.MX6Q, by CSI_DAT[8] to CSI_DAT[19], right?  And, how to convert Bayer RGB format data to RGB / YUV format by i.MX6Q IPU module?

fei.shen@nxp.com
ラベル(3)
0 件の賞賛
返信
1 解決策
1,705件の閲覧回数
Yuri
NXP Employee
NXP Employee

For possible sensor connections, please look at the datasheet(s),

for example - Table 64 (Camera Input Signal Cross Reference, Format, and Bits Per Cycle)

of IMX6DQCEC, Rev. 1, 11/2012.

Software operations are described in Platform SDK (IPU driver, IC tasks).


https://www.freescale.com/webapp/Download?colCode=i.MX6_PLATFORM_SDK&location=null


Also the next may be useful :


https://community.freescale.com/message/309833#309833

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,706件の閲覧回数
Yuri
NXP Employee
NXP Employee

For possible sensor connections, please look at the datasheet(s),

for example - Table 64 (Camera Input Signal Cross Reference, Format, and Bits Per Cycle)

of IMX6DQCEC, Rev. 1, 11/2012.

Software operations are described in Platform SDK (IPU driver, IC tasks).


https://www.freescale.com/webapp/Download?colCode=i.MX6_PLATFORM_SDK&location=null


Also the next may be useful :


https://community.freescale.com/message/309833#309833

0 件の賞賛
返信