1080i de-interlance support for iMX53, based on L2.6.35_11.09.01 BSP -blog archive

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

1080i de-interlance support for iMX53, based on L2.6.35_11.09.01 BSP -blog archive

3,964 次查看
qiang_li-mpu_se
NXP Employee
NXP Employee

    Due to IM53 IPU VDIC hardware limitation, the input and output size for VDIC is 968*1024, so for 1080i, it can't be supported ditectly, we need use split mode to support 1080i de-interlance.

 

IPU lib to support VDI split mode:

ER1109_ipu_lib_vdi_split_support.zip

 

Updated ipu lib source code: imx-lib-11.09.01\ipu\mxc_ipu_hl_lib.c;

Updated vpu unit test code: imx-test-11.09.01\test\mxc_vpu_test

Test command (d1.mp2 is the interlanced MPEG2 RAW video; 1080i.mp4 is the interlanced H.264 RAW video):

    ./mxc_vpu_test.out -D "-i /d1.mp2 -x 1 -f 4 -v h -w 1920 -h 1080"

    ./mxc_vpu_test.out -D "-i /1080i.264 -x 1 -f 2 -v h -w 1920 -h 1080"

 

 

Kernel V4L2 driver to support VDI split mode:

ER1109_v4l2_VDI_Split_patch.zip

 

vdi_split.patch is the kernel patch;

mxc_v4l2_output.c is the patched kernel source code file "linux-2.6.35.3\drivers\media\video\mxc\output\mxc_v4l2_output.c".

Test command (d1.mp2 is the interlanced MPEG2 RAW video; 1080i.mp4 is the interlanced H.264 RAW video):

    ./mxc_vpu_test.out -D "-i /d1.mp2 -x 0 -f 4 -v h -w 1920 -h 1080"

    ./mxc_vpu_test.out -D "-i /1080i.264 -x 0 -f 2 -v h -w 1920 -h 1080"

Original Attachment has been moved to: 22-ER1109_ipu_lib_vdi_split_support.zip

Original Attachment has been moved to: 23-ER1109_v4l2_VDI_Split_patch.zip

标记 (1)
0 项奖励
回复
5 回复数

2,852 次查看
phil_martin
Contributor II

Can this be made to support the imx6?

- i'm really interested in 1080i->1080p @ 60Hz on the imx6

Thanks

0 项奖励
回复

2,852 次查看
qiang_li-mpu_se
NXP Employee
NXP Employee

The default iMX6 BSP supports it.

0 项奖励
回复

2,852 次查看
phil_martin
Contributor II

Thanks for your reply Qiang Li

So, just to confirm, this patch supports 1080i -> 1080p / 60 on the imx6?

- can you provide a link to the correct BSP?

Thanks

0 项奖励
回复

2,852 次查看
stevetsai
Contributor III

Could I know what's device we can test your codes? I'd like to test video input with 720p or 1080i on i.mx53, but I could not find the device to test.  Thanks.

0 项奖励
回复

2,852 次查看
qiang_li-mpu_se
NXP Employee
NXP Employee

You can test it on iMX53 QSB board with VGA output.

0 项奖励
回复