1. Could we Tristate the UART Pins and Pins Mentioned below in Snapshot (See snapshot of schematic for Reference).We are using these Pins for interface with RF Module and Antenna Module .So, Is there any Hardware mechanism so that we can Tri-State these

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

1. Could we Tristate the UART Pins and Pins Mentioned below in Snapshot (See snapshot of schematic for Reference).We are using these Pins for interface with RF Module and Antenna Module .So, Is there any Hardware mechanism so that we can Tri-State these

641件の閲覧回数
arunmantoo
Contributor I

pastedImage_1.png

0 件の賞賛
返信
1 返信

572件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi ARUN

there is no tri-state functionality on i.MX6DQ pad, one can
use open drain, ODE bit11 IOMUXC_SW_PAD_CTL_PAD_x_y register
described in IOMUX Chapter of i.MX6DQ Reference Manual
https://www.nxp.com/docs/en/reference-manual/IMX6DQRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信