1.8V simulation of RGMII interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1.8V simulation of RGMII interface

1,857 Views
inmaku
Contributor III

I need to do SI simulation on teh RGMII Interface and use the current i.MX6Q IBIS model together with the appropriate IBIS model of the connected PHY.

The PHA as well as the i.MX6 can operate in 1.8V, 2.5V and 3.3V signbaling - but the IBIS model of teh i.MX6 has only 2.5V Output Driver models

Are there any intentions to add those lower voltages to teh model or do I Need to model with 2.5 and assume, that the results will be similar with 1.8V signaling?

Labels (2)
Tags (3)
0 Kudos
Reply
1 Reply

1,682 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Ingo,

    It is no problem for you to use 2.5V to do simulation. Result is not affected by voltage of RGMII.  Several days ago, a customer used a 1.8V-PHY manufactured by Realtek, and no any problem.

Have a nice day!

Best regards,

Weidong

0 Kudos
Reply