0ohm registor at DRAM_SDCLK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

0ohm registor at DRAM_SDCLK

2,412 Views
T_I
Contributor I

Hi

 

We design our custom board based on MCIMX53-START-R & MCIMX53SMD. DRAM_SDCLK has a series  terminator (0ohm). What meaning does this have?  If not necessary, I want to remove the resistor for space of the board.

regurds,

53-ddr.jpg

0 Kudos
Reply
3 Replies

2,245 Views
T_I
Contributor I

Hi

Thanks for the reply.

I understand their meaning. 

0 Kudos
Reply

2,245 Views
NicolasIzquierd
Contributor III

Hi...

Totally agree with Yuri, those are access points and possibly resistor to compensate the signals due the pcb fabrication,so,  I do not recommend to remove them.

0 Kudos
Reply

2,245 Views
Yuri
NXP Employee
NXP Employee

First - the resistors may serve as test points for probe to analyze waveforms.
Next - if real (SDCLK) signal on the board appears to be not very "good" - it will be possible
to improve situation by locating more suitable termination resistors.
So, it may be recommended to use them at least for prototype design. 

0 Kudos
Reply