ov5640 support on imx8mp

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ov5640 support on imx8mp

ov5640 support on imx8mp

Recently many customers have been tested ov5640 on imx8mp and found different issues, this document point some dtb file issues and simple introduce how to test ov5640 on the imx8mp evk board.

as we known, current bsp supports ov5640, ov2775 and basler camera, and many customers have ov5640 already, so we can test this first

One can find different camera support dtb files for ov5640,

 imx8mp-evk-basler-ov5640.dts

<https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8mp-evk-b...>

imx8mp-evk-ov2775-ov5640.dts

<https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8mp-evk-o...>

 

  • One ov5640 support

 

 

joanxie_0-1625909772678.pngjoanxie_1-1625909803980.png

 

Refer to the imx8mp evk baseboard schematic, we can find camera 1# and camera 2# share the same reset and power down pins

 

joanxie_2-1625909895563.png

 

 

joanxie_3-1625909912412.png

 

joanxie_4-1625909931675.png

 

Refer to the schematic, current evk uses gpio2_IO11 as power down pin and gpio1_IO06 as reset pin, but let’s see the i.mx8mp-evk.dts file

<https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8mp-evk.d...>

ov5640_1: ov5640_mipi@3c {

               compatible = "ovti,ov5640";

               reg = <0x3c>;

               pinctrl-names = "default";

               pinctrl-0 = <&pinctrl_csi0_pwn>, <&pinctrl_csi0_rst>, <&pinctrl_csi_mclk>;

               clocks = <&clk IMX8MP_CLK_IPP_DO_CLKO2>;

               clock-names = "xclk";

               assigned-clocks = <&clk IMX8MP_CLK_IPP_DO_CLKO2>;

               assigned-clock-parents = <&clk IMX8MP_CLK_24M>;

               assigned-clock-rates = <24000000>;

               csi_id = <0>;

               powerdown-gpios = <&gpio4 1 GPIO_ACTIVE_HIGH>;

               reset-gpios = <&gpio4 0 GPIO_ACTIVE_LOW>;

               mclk = <24000000>;

               mclk_source = <0>;

               mipi_csi;

               status = "disabled";

 

               port {

                       ov5640_mipi_1_ep: endpoint {

                               remote-endpoint = <&mipi_csi1_ep>;

                               data-lanes = <1 2>;

                               clock-lanes = <0>;

                       };

               };

        };

 

 

So if customer wants connect I2C3 to ov5640, don’t forget change the power down pin and reset pin as what schematic defines

 

Then you can find the issue obviously in this dts file, and pls try to correct as below:

https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8mp-evk-o...

 

&i2c3 {       

      /delete-node/ov2775_mipi@36;

}; 

&ov5640_1 {

-       pinctrl-0 = <&pinctrl_csi1_pwn>, <&pinctrl_csi1_rst>, <&pinctrl_csi_mclk>;

+      powerdown-gpios = <&gpio2 11 GPIO_ACTIVE_HIGH>;

 +      reset-gpios = <&gpio1 6 GPIO_ACTIVE_LOW>;        

         csi_id = <1>;        

      status = "okay";

};

 

That’s why some customers tested ov5640 by imx8mp-evk-ov2775-ov5640.dts file failed

 

  • Dual ov5640

 

Because ov5640 has ISP, so current bsp connect ov5640 by ISI, so customer can set status of &isi_0 or &isi_1 to “Okay” in the dts file if you just connect one ov5640, Because of evk HW limitation, current board couldn’t support dual ISI, which mean couldn't support dual ov5640, because they share the same power down pin and reset pin, so customer only can connect ov5640 by ISI0 or ISI1 to test 

 

 

无评分
版本历史
最后更新:
‎07-10-2021 02:53 AM
更新人: