iMX8QXP: Reference patch for LCDIF output YUV422 8 bits display mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8QXP: Reference patch for LCDIF output YUV422 8 bits display mode

iMX8QXP: Reference patch for LCDIF output YUV422 8 bits display mode

Use case:

iMX8QXP system can be a video input source to another system.

 

Hardware Pins:

LCDIF_D00 ~ LCDIF_D07

LCDIF_CLK

LCDIF_VSYNC

LCDIF_HSYNC

LCDIF_EN

 

Reference patch:

It is based on L5.4.70_2.3.0 GA BSP. 

File: L5.4.70_2.3.0-iMX8QXP-LCDIF-add-YUV422-8-bits-output.patch

Customer can change the timing parameters in file "panel-lcdif-yuv422.c" as needed, the default timing is a 1280x720 P30 mode:

static const struct display_timing yuv422_lcd_timing = {
    .pixelclock = { 74250000, 74250000, 74250000 },
    .hactive = { 1280, 1280, 1280 },
    .hfront_porch = { 220, 220, 220 },
    .hback_porch = { 110, 110, 110 },
    .hsync_len = { 40, 40, 40 },
    .vactive = { 720, 720, 720 },
    .vfront_porch = { 20, 20, 20 },
    .vback_porch = { 5, 5, 5 },
    .vsync_len = { 5, 5, 5 },
    .flags = DISPLAY_FLAGS_DE_HIGH,
};

 

Test application:

drm_test_yuv.zip: it can set framebuffer to UYVY mode, in this case, no CSC is needed, the data in framebuffer memory will be same as output on display data interface.

drm_test_rgb.zip: it can set framebuffer to RGBA mode, in this case, RGB to YUV CSC is needed, application can draw RGB data into framebuffer as normal, the LCDIF will convert it to YUV422 format on the fly, then output the YUV data to display interface.

 

 

Labels (1)
Attachments
No ratings
Version history
Last update:
‎09-27-2021 03:17 AM
Updated by: