[iMX8QM] How to enable the HDMI RX on L5.10.52_2.1.0 BSP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[iMX8QM] How to enable the HDMI RX on L5.10.52_2.1.0 BSP

[iMX8QM] How to enable the HDMI RX on L5.10.52_2.1.0 BSP

 

From L5.4 BSP, the iMX8QM HDMI RX feature is removed from BSP, but it is added back in L5.10.52 2.1.0 BSP. The followed is the detail steps to use HDMI RX.

 

  1. We need enable the followed kernel config to make hdmirx driver work:

    CONFIG_IMX8_MEDIA_DEVICE=y
    CONFIG_MHDP_HDMIRX=y

  1. apply the attached kernel patch.
  2. put hdmi firmware “hdmirxfw.bin” and “hdmitxfw.bin” to SD card’s FAT partition
  3. test command:

    gst-launch-1.0 v4l2src device=/dev/video2 ! autovideosink

 

Note: To test the hdmi feature, the display should also use the HDMI TX. And in Uboot, to load the hdmirx firmware, we can run the followed commands first, then run the "boot" command:

    run loadhdprx
    hdprx load 0x9c800000
    setenv fdt_file imx8qm-mek-hdmi-rx.dtb

 

添付
評価なし
バージョン履歴
最終更新日:
‎11-04-2021 07:28 PM
更新者: