i.MX6SX Register Programming Aids

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6SX Register Programming Aids

i.MX6SX Register Programming Aids

Important: If you have any questions or would like to report any issues with the DDR tools or supporting documents please create a support ticket in the i.MX community. Please note that any private messages or direct emails are not monitored and will not receive a response.

 

This is a detailed programming aid for the registers associated with MMDC initialization. The last sheet formats the register settings for use with ARM RealView ICE. It can also be used with the windows executable for the DDR Stress Test. This programming aid was used for internal NXP validation boards.

标签 (1)
附件
评论

Register MMDC_MAARCR is not normally programmed by the initialization script. Freescale recommends leaving it with default values.

This is an advisory to customers who decide to change some of the fields in this register.

A bug has been found with the ARCR_GUARD field. It should always be left programmed to the default 0x0 value. If programmed to a different value, the behavior is unpredictable.

100% 有帮助 (1/1)
版本历史
最后更新:
‎05-04-2021 01:40 PM
更新人: