i.MX 93 Memory Compatibility Guide

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 93 Memory Compatibility Guide

i.MX 93 Memory Compatibility Guide

The purpose of this document is to provide extended guidance for the selection of compatible LPDDR4/4X memory devices that are supported by the i.MX 93 series of processors. In all cases, it is strongly recommended to follow the DRAM layout guidelines outlined in the NXP Hardware Developer's Guides for the specific SoCs.

The i.MX 93 series of processors supports different packages, and each have their own maximum supported LPDDR4/4x data rates. Please refer to the respective datasheets.

Memory devices with binary densities (e.g., 1 GB, 2 GB, 4 GB) are preferred because they simplify memory management by aligning with system addressing schemes and reducing software complexity.

NOTE: Some of the LPDDR4/4X devices may not support operation at low speeds and in addition, DQ ODT may not be active, which can impact signal integrity at these speeds. If low-speed operation is planned in the use case, please consult with the memory vendor about the configuration aspects and possible customization of the memory device so correct functionality is ensured.

LPDDR4/4X - Maximum Supported Densities

SoC Max Data bus width Maximum density Assumed memory organization Notes

i.MX 93

(i.MX 93xx)

16-bit 16 Gb / (2 GB) single rank, single channel device with 17-row addresses (R0 - R16) 1, 2, 3

 

LPDDR4/4X - List of Validated Memories

The validation process is an ongoing effort - regular updates of the table are expected.

SoC Density Memory Vendor Validated Memory Part# Notes
i.MX 93














16 Gb/ (2 GB) Micron

LPDDR4/4x:

MT53E1G16D1FW-046 AAT:A 

(Z32N)

MT53E1G16D1ZW-046 AAT:C (Z42N)

7

 

4, 8

8 Gb/ (1 GB) Micron

LPDDR4/4x:

MT53D512M16D1DS-046 AAT (Z11M)

4, 10
16 Gb/ (2 GB) Micron

LPDDR4/4x:

MT53E1G32D2FW-046 AUT:B (Z42M)

4, 5, 10
8 Gb/ (1 GB)

Nanya

LPDDR4:

NT6AN512M16AV-J1I

LPDDR4x:

NT6AP512M16BV-J1I

4, 8
4 Gb/ (512 MB)

Nanya

LPDDR4x:

NT6AP256M16AV 

4, 8
16 Gb/ (2 GB)

Kingston

LPDDR4:

D1611PM3BDGUI-U

4, 8
16 Gb/ (2 GB)

Kingston

LPDDR4:

C1612PC2WDGTKR-U 

7, 9
4 Gb/ (512 MB)

ISSI

LPDDR4:

IS43LQ16256B-062BLI

4, 8
2 Gb / (256 MB)

ISSI

LPDDR4:

IS43LQ16128A-062BSLI

4, 6, 8
  8 Gb/ (1 GB)

CXMT

LPDDR4/4x:

CXDB4CBAM-EA-M

4, 9
16 Gb/ (2 GB)

JSC

LPDDR4x:

JSL4BAG167ZAMF 

4, 8
8 Gb/ (1 GB)

JSC

LPDDR4x:

JSL4B8G168ZAMF-05x 

4, 8
4 Gb/ (512 MB)

JSC

LPDDR4x:

JSL4A4G168ZAMF-05

4, 8
2 Gb / (256 MB)

Winbond

 LPDDR4x:

W66BQ6NBHAGJ

4, 6, 8
8 Gb / (1 GB)

IM

(Intelligent Memory)

LPDDR4x:

IM8G16L4JCB-046I

4, 11
16 Gb / (2 GB)

IM

(Intelligent Memory)

LPDDR4/4x:

IMAG16L4KBBG

4, 8
4 Gb / (512 MB)

Samsung

LPDDR4:

K4F4E164HD-THCL

4, 8
8Gb / (1 GB)

AM

(Alliance Memory)

LPDDR4X:

AS4C512M16MD4V-053BIN

4, 8
4 Gb / (512 MB)

ISSI

LPDDR4/4X:

IS43LQ16256B-053BLI

4, 8
8 Gb / (1 GB)

ISSI

LPDDR4/4X:

IS46LQ16512B-046BLA2

4, 8

32Gb / (4GB)

16 Gb / (2Gb) usable by i.MX 93

ISSI

LPDDR4/4X:

IS46LQ32K01B-046BLI

4, 8

 

Note 1:

The numbers are based purely on the IP documentation for the DDR Controller and the DDR PHY, on the settings of the implementation parameters chosen for their integration into the SoC, SoC reference manual and on the JEDEC standards JESD209-4B/JESD209-4-1 (LPDDR4/4X). Therefore, they are not backed by validation, unless said otherwise and there is no guarantee that an SoC with the specific density and/or desired internal organization is offered by the memory vendors. Should the customers choose to use the maximum density and assume it in the intended use case, they do it at their own risk.

Note 2:

Byte-mode LPDDR4/4X devices (x16 channel internally split between two dies, x8 each) of any density are not supported therefore, the numbers are applicable only to devices with x16 internal organization (referred to as "standard" in the JEDEC specification).

Note 3:

The SoC also supports dual rank single channel devices therefore, 16Gb/2GB density can be also achieved by using a dual rank single channel device with 16-row addresses (R0 - R15).

Note 4:

The memory part number did not undergo full JEDEC verification however, it passed all functional testing items.

Note 5:

This is a dual channel x32 device. Since i.MX93 only supports 16-bit LPDDR4/X data bus, it can only interface with one of the channels and therefore, utilize only half of the device's density. As indicated in the table - the device has 32Gb/4GB density however, only 16Gb/2GB can be used. There is no functional problem with using only one channel of a dual channel device as the channels are independent in LPDDR4/4X. 

Note 6:

This is a new JEDEC 100 ball package, half the size of the standard 200 ball package. This 100 ball package has the same performance and functionality as the 200 ball package, and has the added advantage of being smaller and cheaper than the standard package.

Note 7:

This device has been EoLed by the manufacturer and has been updated by a new memory part number 

Note 8:

Part is active. Reviewed Q3 2026

Note 9:

Part is obsolete.

Note 10:

This device will be EoLed in Q2 24 by the manufacturer and will not be updated by a new memory part number

Note 11:

DQ eye marginalities were identified during TSA analysis. vTSA and stability testing did not identify any issues.

%3CLINGO-SUB%20id%3D%22lingo-sub-1725656%22%20slang%3D%22en-US%22%20mode%3D%22UPDATE%22%3Ei.MX%2093%20Memory%20Compatibility%20Guide%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-1725656%22%20slang%3D%22en-US%22%20mode%3D%22UPDATE%22%3E%0A%3CP%3E%3CSPAN%3EThe%20purpose%20of%20this%20document%20is%20to%20provide%20extended%20guidance%20for%20the%20selection%20of%20compatible%20LPDDR4%2F4X%20memory%20devices%20that%20are%20supported%20by%20the%20i.MX%2093%20series%20of%20processors.%26nbsp%3BIn%20all%20cases%2C%20it%20is%20strongly%20recommended%20to%20follow%20the%20DRAM%20layout%20guidelines%20outlined%20in%20the%20NXP%20Hardware%20Developer's%20Guides%20for%20the%20specific%20SoCs.%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%3E%3CSPAN%3EThe%20i.MX%2093%20series%20of%20processors%20supports%20different%20packages%2C%20and%20each%20have%20their%20own%20maximum%20supported%20LPDDR4%2F4x%20data%20rates.%20Please%20refer%20to%20the%20respective%20datasheets.%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%3E%3CSPAN%3EMemory%20devices%20with%20binary%20densities%20(e.g.%2C%201%20GB%2C%202%20GB%2C%204%20GB)%20are%20preferred%20because%20they%20simplify%20memory%20management%20by%20aligning%20with%20system%20addressing%20schemes%20and%20reducing%20software%20complexity.%3C%2FSPAN%3E%3C%2FP%3E%0A%3CP%3E%3CFONT%20size%3D%222%22%3E%3CSTRONG%3ENOTE%3A%3C%2FSTRONG%3E%20%3CFONT%20color%3D%22%230000FF%22%3ESome%20of%20the%20LPDDR4%2F4X%20devices%20may%20not%20support%20operation%20at%20low%20speeds%20and%20in%20addition%2C%20DQ%20ODT%20may%20not%20be%20active%2C%20which%20can%20impact%20signal%20integrity%20at%20these%20speeds.%20If%20low-speed%20operation%20is%20planned%20in%20the%20use%20case%2C%20please%20consult%20with%20the%20memory%20vendor%20about%20the%20configuration%20aspects%20and%20possible%20customization%20of%20the%20memory%20device%20so%20correct%20functionality%20is%20ensured.%3C%2FFONT%3E%3C%2FFONT%3E%3C%2FP%3E%0A%3CH3%20id%3D%22toc-hId-1255326383%22%20id%3D%22toc-hId-1997896850%22%3ELPDDR4%2F4X%20-%20Maximum%20Supported%20Densities%3C%2FH3%3E%0A%3CTABLE%20border%3D%221%22%20width%3D%22100%25%22%3E%0A%3CTBODY%3E%0A%3CTR%20style%3D%22background-color%3A%20cyan%3B%22%3E%0A%3CTD%20width%3D%2220%25%22%20height%3D%2269px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%3CSTRONG%3ESoC%3C%2FSTRONG%3E%3C%2FTD%3E%0A%3CTD%20width%3D%2220%25%22%20height%3D%2269px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%3CSTRONG%3EMax%20Data%20bus%20width%3C%2FSTRONG%3E%3C%2FTD%3E%0A%3CTD%20width%3D%2220%25%22%20height%3D%2269px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%3CSTRONG%3EMaximum%20density%3C%2FSTRONG%3E%3C%2FTD%3E%0A%3CTD%20width%3D%2220%25%22%20height%3D%2269px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%3CSTRONG%3EAssumed%20memory%20organization%3C%2FSTRONG%3E%3C%2FTD%3E%0A%3CTD%20width%3D%2220%25%22%20height%3D%2269px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%3CSTRONG%3ENotes%3C%2FSTRONG%3E%3C%2FTD%3E%0A%3C%2FTR%3E%0A%3CTR%3E%0A%3CTD%20width%3D%2220%25%22%20height%3D%22113px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%0A%3CP%3E%3CSTRONG%3Ei.MX%2093%3C%2FSTRONG%3E%3C%2FP%3E%0A%3CP%3E(i.MX%2093xx)%3C%2FP%3E%0A%3C%2FTD%3E%0A%3CTD%20width%3D%2220%25%22%20height%3D%22113px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E16-bit%3C%2FTD%3E%0A%3CTD%20width%3D%2220%25%22%20height%3D%22113px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E16%20Gb%20%2F%20(2%20GB)%3C%2FTD%3E%0A%3CTD%20width%3D%2220%25%22%20height%3D%22113px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3Esingle%20rank%2C%20single%20channel%20device%20with%2017-row%20addresses%20(R0%20-%20R16)%3C%2FTD%3E%0A%3CTD%20width%3D%2220%25%22%20height%3D%22113px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E1%2C%202%2C%203%3C%2FTD%3E%0A%3C%2FTR%3E%0A%3C%2FTBODY%3E%0A%3C%2FTABLE%3E%0A%3CH3%20id%3D%22toc-hId--552128080%22%20id%3D%22toc-hId-190442387%22%3E%26nbsp%3B%3C%2FH3%3E%0A%3CH3%20id%3D%22toc-hId-1935384753%22%20id%3D%22toc-hId--1617012076%22%3ELPDDR4%2F4X%20-%20List%20of%20Validated%20Memories%3C%2FH3%3E%0A%3CP%3E%3CSPAN%3EThe%20validation%20process%20is%20an%20ongoing%20effort%20-%20regular%20updates%20of%20the%20table%20are%20expected.%3C%2FSPAN%3E%3C%2FP%3E%0A%3CTABLE%20style%3D%22width%3A%20100%25%3B%22%20border%3D%221%22%20width%3D%22100%25%22%3E%0A%3CTBODY%3E%0A%3CTR%20style%3D%22background-color%3A%20cyan%3B%20height%3A%2069px%3B%22%3E%0A%3CTD%20width%3D%2211.455331412103748%25%22%20height%3D%2269px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%3CSTRONG%3ESoC%3C%2FSTRONG%3E%3C%2FTD%3E%0A%3CTD%20width%3D%2213.32853025936599%25%22%20height%3D%2269px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%3CSTRONG%3EDensity%3C%2FSTRONG%3E%3C%2FTD%3E%0A%3CTD%20width%3D%2215.760086455331408%25%22%20height%3D%2269px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%3CSTRONG%3EMemory%20Vendor%3C%2FSTRONG%3E%3C%2FTD%3E%0A%3CTD%20width%3D%2221.95605187319885%25%22%20height%3D%2269px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%3CSTRONG%3EValidated%20Memory%20Part%23%3C%2FSTRONG%3E%3C%2FTD%3E%0A%3CTD%20width%3D%2212.5%25%22%20height%3D%2269px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%3CSTRONG%3ENotes%3C%2FSTRONG%3E%3C%2FTD%3E%0A%3C%2FTR%3E%0A%3CTR%3E%0A%3CTD%20rowspan%3D%2221%22%20width%3D%2211.455331412103748%25%22%20height%3D%221763px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%3CSTRONG%3Ei.MX%2093%3C%2FSTRONG%3E%3CBR%20%2F%3E%3CSTRONG%3E%3CBR%20%2F%3E%3C%2FSTRONG%3E%3CSTRONG%3E%3CBR%20%2F%3E%3C%2FSTRONG%3E%3CSTRONG%3E%3CBR%20%2F%3E%3C%2FSTRONG%3E%3CSTRONG%3E%3CBR%20%2F%3E%3C%2FSTRONG%3E%3CSTRONG%3E%3CBR%20%2F%3E%3C%2FSTRONG%3E%3CSTRONG%3E%3CBR%20%2F%3E%3C%2FSTRONG%3E%3CSTRONG%3E%3CBR%20%2F%3E%3C%2FSTRONG%3E%3CSTRONG%3E%3CBR%20%2F%3E%3C%2FSTRONG%3E%3CSTRONG%3E%3CBR%20%2F%3E%3C%2FSTRONG%3E%3CSTRONG%3E%3CBR%20%2F%3E%3C%2FSTRONG%3E%3CSTRONG%3E%3CBR%20%2F%3E%3C%2FSTRONG%3E%3CSTRONG%3E%3CBR%20%2F%3E%3C%2FSTRONG%3E%3CSTRONG%3E%3CBR%20%2F%3E%3C%2FSTRONG%3E%3CSTRONG%3E%3CBR%20%2F%3E%3C%2FSTRONG%3E%3C%2FTD%3E%0A%3CTD%20width%3D%2213.32853025936599%25%22%20height%3D%22178px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E16%20Gb%2F%20(2%20GB)%3C%2FTD%3E%0A%3CTD%20width%3D%2215.760086455331408%25%22%20height%3D%22178px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3EMicron%3C%2FTD%3E%0A%3CTD%20width%3D%2221.95605187319885%25%22%20height%3D%22178px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%0A%3CP%3E%3CSTRONG%3E%3CFONT%20size%3D%222%22%3ELPDDR4%2F4x%3A%20%3C%2FFONT%3E%3C%2FSTRONG%3E%3C%2FP%3E%0A%3CP%3E%3CFONT%20size%3D%222%22%3EMT53E1G16D1FW-046%20AAT%3AA%26nbsp%3B%3C%2FFONT%3E%3C%2FP%3E%0A%3CP%3E%3CFONT%20size%3D%222%22%3E(Z32N)%3C%2FFONT%3E%3C%2FP%3E%0A%3CP%3E%3CFONT%20size%3D%222%22%3EMT53E1G16D1%3CSTRONG%3EZ%3C%2FSTRONG%3EW-046%20AAT%3AC%20(Z42N)%3C%2FFONT%3E%3C%2FP%3E%0A%3C%2FTD%3E%0A%3CTD%20width%3D%2212.5%25%22%20height%3D%22178px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%0A%3CP%3E7%3C%2FP%3E%0A%3CBR%20%2F%3E%0A%3CP%3E4%2C%208%3C%2FP%3E%0A%3C%2FTD%3E%0A%3C%2FTR%3E%0A%3CTR%3E%0A%3CTD%20width%3D%2213.32853025936599%25%22%20height%3D%22102px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E8%20Gb%2F%20(1%20GB)%3C%2FTD%3E%0A%3CTD%20width%3D%2215.760086455331408%25%22%20height%3D%22102px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3EMicron%3C%2FTD%3E%0A%3CTD%20width%3D%2221.95605187319885%25%22%20height%3D%22102px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%0A%3CP%3E%3CSTRONG%3E%3CFONT%20size%3D%222%22%3ELPDDR4%2F4x%3A%3C%2FFONT%3E%3C%2FSTRONG%3E%3C%2FP%3E%0A%3CP%3E%3CFONT%20size%3D%222%22%3EMT53D512M16D1DS-046%20AAT%20(Z11M)%3C%2FFONT%3E%3C%2FP%3E%0A%3C%2FTD%3E%0A%3CTD%20width%3D%2212.5%25%22%20height%3D%22102px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E4%2C%2010%3C%2FTD%3E%0A%3C%2FTR%3E%0A%3CTR%3E%0A%3CTD%20width%3D%2213.32853025936599%25%22%20height%3D%22102px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E16%20Gb%2F%20(2%20GB)%3C%2FTD%3E%0A%3CTD%20width%3D%2215.760086455331408%25%22%20height%3D%22102px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3EMicron%3C%2FTD%3E%0A%3CTD%20width%3D%2221.95605187319885%25%22%20height%3D%22102px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%0A%3CP%3E%3CSTRONG%3E%3CFONT%20size%3D%222%22%3ELPDDR4%2F4x%3A%20%3C%2FFONT%3E%3C%2FSTRONG%3E%3C%2FP%3E%0A%3CP%3E%3CFONT%20size%3D%222%22%3EMT53E1G32D2FW-046%20AUT%3AB%20(Z42M)%3C%2FFONT%3E%3C%2FP%3E%0A%3C%2FTD%3E%0A%3CTD%20width%3D%2212.5%25%22%20height%3D%22102px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E4%2C%205%2C%2010%3C%2FTD%3E%0A%3C%2FTR%3E%0A%3CTR%3E%0A%3CTD%20width%3D%2213.32853025936599%25%22%20height%3D%22155px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E8%20Gb%2F%20(1%20GB)%3C%2FTD%3E%0A%3CTD%20width%3D%2215.760086455331408%25%22%20height%3D%22155px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%0A%3CP%3ENanya%3C%2FP%3E%0A%3C%2FTD%3E%0A%3CTD%20width%3D%2221.95605187319885%25%22%20height%3D%22155px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%0A%3CP%3E%3CSTRONG%3E%3CFONT%20size%3D%222%22%3ELPDDR4%3A%20%3C%2FFONT%3E%3C%2FSTRONG%3E%3C%2FP%3E%0A%3CP%3E%3CFONT%20size%3D%222%22%3ENT6AN512M16AV-J1I%3C%2FFONT%3E%3C%2FP%3E%0A%3CP%3E%3CSTRONG%3E%3CFONT%20size%3D%222%22%3ELPDDR4x%3A%3C%2FFONT%3E%3C%2FSTRONG%3E%3C%2FP%3E%0A%3CP%3E%3CFONT%20size%3D%222%22%3ENT6AP512M16BV-J1I%3C%2FFONT%3E%3C%2FP%3E%0A%3C%2FTD%3E%0A%3CTD%20width%3D%2212.5%25%22%20height%3D%22155px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E4%2C%208%3C%2FTD%3E%0A%3C%2FTR%3E%0A%3CTR%3E%0A%3CTD%20width%3D%2213.32853025936599%25%22%20height%3D%2279px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E4%20Gb%2F%20(512%20MB)%3C%2FTD%3E%0A%3CTD%20width%3D%2215.760086455331408%25%22%20height%3D%2279px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%0A%3CP%3ENanya%3C%2FP%3E%0A%3C%2FTD%3E%0A%3CTD%20width%3D%2221.95605187319885%25%22%20height%3D%2279px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%0A%3CP%3E%3CSTRONG%3E%3CFONT%20size%3D%222%22%3ELPDDR4x%3A%3C%2FFONT%3E%3C%2FSTRONG%3E%3C%2FP%3E%0A%3CP%3E%3CFONT%20size%3D%222%22%3ENT6AP256M16AV%26nbsp%3B%3C%2FFONT%3E%3C%2FP%3E%0A%3C%2FTD%3E%0A%3CTD%20width%3D%2212.5%25%22%20height%3D%2279px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E4%2C%208%3C%2FTD%3E%0A%3C%2FTR%3E%0A%3CTR%3E%0A%3CTD%20width%3D%2213.32853025936599%25%22%20height%3D%2279px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E16%20Gb%2F%20(2%20GB)%3C%2FTD%3E%0A%3CTD%20width%3D%2215.760086455331408%25%22%20height%3D%2279px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%0A%3CP%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3EKingston%3C%2FP%3E%0A%3C%2FTD%3E%0A%3CTD%20width%3D%2221.95605187319885%25%22%20height%3D%2279px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%0A%3CP%3E%3CSTRONG%3E%3CFONT%20size%3D%222%22%3E%3CSPAN%20class%3D%22NormalTextRun%20SCXW218536227%20BCX8%22%20data-ccp-parastyle%3D%22No%20Spacing%22%3ELPDDR4%3A%3C%2FSPAN%3E%3C%2FFONT%3E%3C%2FSTRONG%3E%3C%2FP%3E%0A%3CP%3E%3CFONT%20size%3D%222%22%3E%3CSPAN%20class%3D%22NormalTextRun%20SCXW218536227%20BCX8%22%20data-ccp-parastyle%3D%22No%20Spacing%22%3ED1611PM3BDGUI-U%3C%2FSPAN%3E%20%3C%2FFONT%3E%3C%2FP%3E%0A%3C%2FTD%3E%0A%3CTD%20width%3D%2212.5%25%22%20height%3D%2279px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E4%2C%208%3C%2FTD%3E%0A%3C%2FTR%3E%0A%3CTR%3E%0A%3CTD%20width%3D%2213.32853025936599%25%22%20height%3D%2279px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E16%20Gb%2F%20(2%20GB)%3C%2FTD%3E%0A%3CTD%20width%3D%2215.760086455331408%25%22%20height%3D%2279px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%0A%3CP%3EKingston%3C%2FP%3E%0A%3C%2FTD%3E%0A%3CTD%20width%3D%2221.95605187319885%25%22%20height%3D%2279px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%0A%3CP%3E%3CSTRONG%3E%3CFONT%20size%3D%222%22%3ELPDDR4%3A%3C%2FFONT%3E%3C%2FSTRONG%3E%3C%2FP%3E%0A%3CP%3E%3CFONT%20size%3D%222%22%3EC1612PC2WDGTKR-U%26nbsp%3B%3C%2FFONT%3E%3C%2FP%3E%0A%3C%2FTD%3E%0A%3CTD%20width%3D%2212.5%25%22%20height%3D%2279px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E7%2C%209%3C%2FTD%3E%0A%3C%2FTR%3E%0A%3CTR%3E%0A%3CTD%20width%3D%2213.32853025936599%25%22%20height%3D%2279px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E4%20Gb%2F%20(512%20MB)%3C%2FTD%3E%0A%3CTD%20width%3D%2215.760086455331408%25%22%20height%3D%2279px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%0A%3CP%3EISSI%3C%2FP%3E%0A%3C%2FTD%3E%0A%3CTD%20width%3D%2221.95605187319885%25%22%20height%3D%2279px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%0A%3CP%3E%3CSTRONG%3E%3CFONT%20size%3D%222%22%3ELPDDR4%3A%3C%2FFONT%3E%3C%2FSTRONG%3E%3C%2FP%3E%0A%3CP%3E%3CFONT%20size%3D%222%22%3EIS43LQ16256B-062BLI%3C%2FFONT%3E%3C%2FP%3E%0A%3C%2FTD%3E%0A%3CTD%20width%3D%2212.5%25%22%20height%3D%2279px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E4%2C%208%3C%2FTD%3E%0A%3C%2FTR%3E%0A%3CTR%3E%0A%3CTD%20width%3D%2213.32853025936599%25%22%20height%3D%2279px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E2%20Gb%20%2F%20(256%20MB)%3C%2FTD%3E%0A%3CTD%20width%3D%2215.760086455331408%25%22%20height%3D%2279px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%0A%3CP%3EISSI%3C%2FP%3E%0A%3C%2FTD%3E%0A%3CTD%20width%3D%2221.95605187319885%25%22%20height%3D%2279px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%0A%3CP%3E%3CSTRONG%3E%3CFONT%20size%3D%222%22%3ELPDDR4%3A%3C%2FFONT%3E%3C%2FSTRONG%3E%3C%2FP%3E%0A%3CP%3E%3CFONT%20size%3D%222%22%3EIS43LQ16128A-062BSLI%3C%2FFONT%3E%3C%2FP%3E%0A%3C%2FTD%3E%0A%3CTD%20width%3D%2212.5%25%22%20height%3D%2279px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E4%2C%206%2C%208%3C%2FTD%3E%0A%3C%2FTR%3E%0A%3CTR%3E%0A%3CTD%20width%3D%2213.32853025936599%25%22%20height%3D%2279px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%26nbsp%3B%208%20Gb%2F%20(1%20GB)%3C%2FTD%3E%0A%3CTD%20width%3D%2215.760086455331408%25%22%20height%3D%2279px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%0A%3CP%3ECXMT%3C%2FP%3E%0A%3C%2FTD%3E%0A%3CTD%20width%3D%2221.95605187319885%25%22%20height%3D%2279px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%0A%3CP%3E%3CSTRONG%3E%3CFONT%20size%3D%222%22%3ELPDDR4%2F4x%3A%3C%2FFONT%3E%3C%2FSTRONG%3E%3C%2FP%3E%0A%3CP%3E%3CFONT%20size%3D%222%22%3ECXDB4CBAM-EA-M%3C%2FFONT%3E%3C%2FP%3E%0A%3C%2FTD%3E%0A%3CTD%20width%3D%2212.5%25%22%20height%3D%2279px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E4%2C%209%3C%2FTD%3E%0A%3C%2FTR%3E%0A%3CTR%3E%0A%3CTD%20width%3D%2213.32853025936599%25%22%20height%3D%2279px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E16%20Gb%2F%20(2%20GB)%3C%2FTD%3E%0A%3CTD%20width%3D%2215.760086455331408%25%22%20height%3D%2279px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%0A%3CP%3EJSC%3C%2FP%3E%0A%3C%2FTD%3E%0A%3CTD%20width%3D%2221.95605187319885%25%22%20height%3D%2279px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%0A%3CP%3E%3CSTRONG%3E%3CFONT%20size%3D%222%22%3ELPDDR4x%3A%3C%2FFONT%3E%3C%2FSTRONG%3E%3C%2FP%3E%0A%3CP%3E%3CFONT%20size%3D%222%22%3EJSL4BAG167ZAMF%26nbsp%3B%3C%2FFONT%3E%3C%2FP%3E%0A%3C%2FTD%3E%0A%3CTD%20width%3D%2212.5%25%22%20height%3D%2279px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E4%2C%208%3C%2FTD%3E%0A%3C%2FTR%3E%0A%3CTR%3E%0A%3CTD%20width%3D%2213.32853025936599%25%22%20height%3D%2279px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E8%20Gb%2F%20(1%20GB)%3C%2FTD%3E%0A%3CTD%20width%3D%2215.760086455331408%25%22%20height%3D%2279px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%0A%3CP%3EJSC%3C%2FP%3E%0A%3C%2FTD%3E%0A%3CTD%20width%3D%2221.95605187319885%25%22%20height%3D%2279px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%0A%3CP%3E%3CSTRONG%3E%3CFONT%20size%3D%222%22%3ELPDDR4x%3A%3C%2FFONT%3E%3C%2FSTRONG%3E%3C%2FP%3E%0A%3CP%3E%3CFONT%20size%3D%222%22%3EJSL4B8G168ZAMF-05x%26nbsp%3B%3C%2FFONT%3E%3C%2FP%3E%0A%3C%2FTD%3E%0A%3CTD%20width%3D%2212.5%25%22%20height%3D%2279px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E4%2C%208%3C%2FTD%3E%0A%3C%2FTR%3E%0A%3CTR%3E%0A%3CTD%20width%3D%2213.32853025936599%25%22%20height%3D%2279px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E4%20Gb%2F%20(512%20MB)%3C%2FTD%3E%0A%3CTD%20width%3D%2215.760086455331408%25%22%20height%3D%2279px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%0A%3CP%3EJSC%3C%2FP%3E%0A%3C%2FTD%3E%0A%3CTD%20width%3D%2221.95605187319885%25%22%20height%3D%2279px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%0A%3CP%3E%3CSTRONG%3E%3CFONT%20size%3D%222%22%3ELPDDR4x%3A%3C%2FFONT%3E%3C%2FSTRONG%3E%3C%2FP%3E%0A%3CP%3E%3CFONT%20size%3D%222%22%3EJSL4A4G168ZAMF-05%3C%2FFONT%3E%3C%2FP%3E%0A%3C%2FTD%3E%0A%3CTD%20width%3D%2212.5%25%22%20height%3D%2279px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E4%2C%208%3C%2FTD%3E%0A%3C%2FTR%3E%0A%3CTR%3E%0A%3CTD%20width%3D%2213.32853025936599%25%22%20height%3D%2279px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E2%20Gb%20%2F%20(256%20MB)%3C%2FTD%3E%0A%3CTD%20width%3D%2215.760086455331408%25%22%20height%3D%2279px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%0A%3CP%3EWinbond%3C%2FP%3E%0A%3C%2FTD%3E%0A%3CTD%20width%3D%2221.95605187319885%25%22%20height%3D%2279px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%0A%3CP%3E%3CSTRONG%3E%3CFONT%20size%3D%222%22%3E%26nbsp%3BLPDDR4x%3A%3C%2FFONT%3E%3C%2FSTRONG%3E%3C%2FP%3E%0A%3CP%3E%3CFONT%20size%3D%222%22%3EW66BQ6NBHAGJ%3C%2FFONT%3E%3C%2FP%3E%0A%3C%2FTD%3E%0A%3CTD%20width%3D%2212.5%25%22%20height%3D%2279px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E4%2C%206%2C%208%3C%2FTD%3E%0A%3C%2FTR%3E%0A%3CTR%3E%0A%3CTD%20width%3D%2213.32853025936599%25%22%20height%3D%2279px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E8%20Gb%20%2F%20(1%20GB)%3C%2FTD%3E%0A%3CTD%20width%3D%2215.760086455331408%25%22%20height%3D%2279px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%0A%3CP%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3EIM%3C%2FP%3E%0A%3CP%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%3CFONT%20size%3D%222%22%3E(Intelligent%20Memory)%3C%2FFONT%3E%3C%2FP%3E%0A%3C%2FTD%3E%0A%3CTD%20width%3D%2221.95605187319885%25%22%20height%3D%2279px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%0A%3CP%3E%3CSTRONG%3E%3CFONT%20size%3D%222%22%3ELPDDR4x%3A%3C%2FFONT%3E%3C%2FSTRONG%3E%3C%2FP%3E%0A%3CP%3E%3CFONT%20size%3D%222%22%3EIM8G16L4JCB-046I%3C%2FFONT%3E%3C%2FP%3E%0A%3C%2FTD%3E%0A%3CTD%20width%3D%2212.5%25%22%20height%3D%2279px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E4%2C%2011%3C%2FTD%3E%0A%3C%2FTR%3E%0A%3CTR%3E%0A%3CTD%20width%3D%2213.32853025936599%25%22%20height%3D%2279px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E16%20Gb%20%2F%20(2%20GB)%3C%2FTD%3E%0A%3CTD%20width%3D%2215.760086455331408%25%22%20height%3D%2279px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%0A%3CP%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3EIM%3C%2FP%3E%0A%3CP%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%3CFONT%20size%3D%222%22%3E(Intelligent%20Memory)%3C%2FFONT%3E%3C%2FP%3E%0A%3C%2FTD%3E%0A%3CTD%20width%3D%2221.95605187319885%25%22%20height%3D%2279px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%0A%3CP%3E%3CSTRONG%3E%3CFONT%20size%3D%222%22%3ELPDDR4%2F4x%3A%3C%2FFONT%3E%3C%2FSTRONG%3E%3C%2FP%3E%0A%3CP%3E%3CFONT%20size%3D%222%22%3EIMAG16L4KBBG%3C%2FFONT%3E%3C%2FP%3E%0A%3C%2FTD%3E%0A%3CTD%20width%3D%2212.5%25%22%20height%3D%2279px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E4%2C%208%3C%2FTD%3E%0A%3C%2FTR%3E%0A%3CTR%3E%0A%3CTD%20width%3D%2213.32853025936599%25%22%20height%3D%2279px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E4%20Gb%20%2F%20(512%20MB)%3C%2FTD%3E%0A%3CTD%20width%3D%2215.760086455331408%25%22%20height%3D%2279px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%0A%3CP%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3ESamsung%3C%2FP%3E%0A%3C%2FTD%3E%0A%3CTD%20width%3D%2221.95605187319885%25%22%20height%3D%2279px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%0A%3CP%3E%3CSTRONG%3E%3CFONT%20size%3D%222%22%3ELPDDR4%3A%3C%2FFONT%3E%3C%2FSTRONG%3E%3C%2FP%3E%0A%3CP%3E%3CFONT%20size%3D%222%22%3EK4F4E164HD-THCL%3C%2FFONT%3E%3C%2FP%3E%0A%3C%2FTD%3E%0A%3CTD%20width%3D%2212.5%25%22%20height%3D%2279px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E4%2C%208%3C%2FTD%3E%0A%3C%2FTR%3E%0A%3CTR%3E%0A%3CTD%20width%3D%2213.32853025936599%25%22%20height%3D%2279px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E8Gb%20%2F%20(1%20GB)%3C%2FTD%3E%0A%3CTD%20width%3D%2215.760086455331408%25%22%20height%3D%2279px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%0A%3CP%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3EAM%3C%2FP%3E%0A%3CP%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%3CFONT%20size%3D%222%22%3E(Alliance%20Memory)%3C%2FFONT%3E%3C%2FP%3E%0A%3C%2FTD%3E%0A%3CTD%20width%3D%2221.95605187319885%25%22%20height%3D%2279px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%0A%3CP%3E%3CSTRONG%3E%3CFONT%20size%3D%222%22%3ELPDDR4X%3A%3C%2FFONT%3E%3C%2FSTRONG%3E%3C%2FP%3E%0A%3CP%3E%3CFONT%20size%3D%222%22%3EAS4C512M16MD4V-053BIN%3C%2FFONT%3E%3C%2FP%3E%0A%3C%2FTD%3E%0A%3CTD%20width%3D%2212.5%25%22%20height%3D%2279px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E4%2C%208%3C%2FTD%3E%0A%3C%2FTR%3E%0A%3CTR%3E%0A%3CTD%20height%3D%2241px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E4%20Gb%20%2F%20(512%20MB)%3C%2FTD%3E%0A%3CTD%20height%3D%2241px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%0A%3CP%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3EISSI%3C%2FP%3E%0A%3C%2FTD%3E%0A%3CTD%20height%3D%2241px%22%3E%0A%3CP%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%3CSTRONG%3E%3CFONT%20size%3D%222%22%3ELPDDR4%2F4X%3A%3C%2FFONT%3E%3C%2FSTRONG%3E%3C%2FP%3E%0A%3CP%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%3CFONT%20size%3D%222%22%3EIS43LQ16256B-053BLI%3C%2FFONT%3E%3C%2FP%3E%0A%3C%2FTD%3E%0A%3CTD%20height%3D%2241px%22%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E4%2C%208%3C%2FTD%3E%0A%3C%2FTR%3E%0A%3CTR%3E%0A%3CTD%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E8%20Gb%20%2F%20(1%20GB)%3C%2FTD%3E%0A%3CTD%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%0A%3CP%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3EISSI%3C%2FP%3E%0A%3C%2FTD%3E%0A%3CTD%3E%0A%3CP%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%3CSTRONG%3E%3CFONT%20size%3D%222%22%3ELPDDR4%2F4X%3A%3C%2FFONT%3E%3C%2FSTRONG%3E%3C%2FP%3E%0A%3CP%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%3CFONT%20size%3D%222%22%3EIS46LQ16512B-046BLA2%3C%2FFONT%3E%3C%2FP%3E%0A%3C%2FTD%3E%0A%3CTD%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E4%2C%208%3C%2FTD%3E%0A%3C%2FTR%3E%0A%3CTR%3E%0A%3CTD%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%0A%3CP%3E32Gb%20%2F%20(4GB)%3C%2FP%3E%0A%3CP%3E%3CFONT%20size%3D%222%22%3E16%20Gb%20%2F%20(2Gb)%20usable%20by%20i.MX%2093%3C%2FFONT%3E%3C%2FP%3E%0A%3C%2FTD%3E%0A%3CTD%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%0A%3CP%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3EISSI%3C%2FP%3E%0A%3C%2FTD%3E%0A%3CTD%3E%0A%3CP%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%3CSTRONG%3E%3CFONT%20size%3D%222%22%3ELPDDR4%2F4X%3A%3C%2FFONT%3E%3C%2FSTRONG%3E%3C%2FP%3E%0A%3CP%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E%3CFONT%20size%3D%222%22%3EIS46LQ32K01B-046BLI%3C%2FFONT%3E%3C%2FP%3E%0A%3C%2FTD%3E%0A%3CTD%20class%3D%22lia-align-center%22%20style%3D%22text-align%3A%20center%3B%22%20style%3D%22text-align%3A%20center%3B%22%3E4%2C%208%3C%2FTD%3E%0A%3C%2FTR%3E%0A%3C%2FTBODY%3E%0A%3C%2FTABLE%3E%0A%3CH3%20class%3D%22lia-align-center%22%20id%3D%22toc-hId-127930290%22%20style%3D%22text-align%3A%20center%3B%22%20id%3D%22toc-hId-870500757%22%20style%3D%22text-align%3A%20center%3B%22%3E%26nbsp%3B%3C%2FH3%3E%0A%3CP%3E%3CSTRONG%3ENote%201%3A%3C%2FSTRONG%3E%3C%2FP%3E%0A%3CP%3E%3CFONT%20size%3D%222%22%3EThe%20numbers%20are%20based%20purely%20on%20the%20IP%20documentation%20for%20the%20DDR%20Controller%20and%20the%20DDR%20PHY%2C%20on%20the%20settings%20of%20the%20implementation%20parameters%20chosen%20for%20their%20integration%20into%20the%20SoC%2C%20SoC%20reference%20manual%20and%20on%20the%20JEDEC%20standards%20JESD209-4B%2FJESD209-4-1%20(LPDDR4%2F4X).%20Therefore%2C%20they%20are%20not%20backed%20by%20validation%2C%20unless%20said%20otherwise%20and%20there%20is%20no%20guarantee%20that%20an%20SoC%20with%20the%20specific%20density%20and%2For%20desired%20internal%20organization%20is%20offered%20by%20the%20memory%20vendors.%20Should%20the%20customers%20choose%20to%20use%20the%20maximum%20density%20and%20assume%20it%20in%20the%20intended%20use%20case%2C%20they%20do%20it%20at%20their%20own%20risk.%3C%2FFONT%3E%3C%2FP%3E%0A%3CP%3E%3CSTRONG%3ENote%202%3A%3C%2FSTRONG%3E%3C%2FP%3E%0A%3CP%3E%3CFONT%20size%3D%222%22%3EByte-mode%20LPDDR4%2F4X%20devices%20(x16%20channel%20internally%20split%20between%20two%20dies%2C%20x8%20each)%20of%20any%20density%20are%20not%20supported%20therefore%2C%20the%20numbers%20are%20applicable%20only%20to%20devices%20with%20x16%20internal%20organization%20(referred%20to%20as%20%22standard%22%20in%20the%20JEDEC%20specification).%3C%2FFONT%3E%3C%2FP%3E%0A%3CP%3E%3CSTRONG%3ENote%203%3A%3C%2FSTRONG%3E%3C%2FP%3E%0A%3CP%3E%3CFONT%20size%3D%222%22%3EThe%20SoC%20also%20supports%20dual%20rank%20single%20channel%20devices%20therefore%2C%2016Gb%2F2GB%20density%20can%20be%20also%20achieved%20by%20using%20a%20dual%20rank%20single%20channel%20device%20with%2016-row%20addresses%20(R0%20-%20R15).%3C%2FFONT%3E%3C%2FP%3E%0A%3CP%3E%3CSTRONG%3ENote%204%3A%3C%2FSTRONG%3E%3C%2FP%3E%0A%3CP%3E%3CFONT%20size%3D%222%22%3EThe%20memory%20part%20number%20did%20not%20undergo%20full%20JEDEC%20verification%20however%2C%20it%20passed%20all%20functional%20testing%20items.%3C%2FFONT%3E%3C%2FP%3E%0A%3CP%3E%3CSTRONG%3ENote%205%3A%3C%2FSTRONG%3E%3C%2FP%3E%0A%3CP%3E%3CFONT%20size%3D%222%22%3EThis%20is%20a%20dual%20channel%20x32%20device.%20Since%20i.MX93%20only%20supports%2016-bit%20LPDDR4%2FX%20data%20bus%2C%20it%20can%20only%20interface%20with%20one%20of%20the%20channels%20and%20therefore%2C%20utilize%20only%20half%20of%20the%20device's%20density.%20As%20indicated%20in%20the%20table%20-%20the%20device%20has%2032Gb%2F4GB%20density%20however%2C%20only%2016Gb%2F2GB%20can%20be%20used.%20There%20is%20no%20functional%20problem%20with%20using%20only%20one%20channel%20of%20a%20dual%20channel%20device%20as%20the%20channels%20are%20independent%20in%20LPDDR4%2F4X.%3C%2FFONT%3E%26nbsp%3B%3C%2FP%3E%0A%3CP%3E%3CSTRONG%3ENote%206%3A%3C%2FSTRONG%3E%3C%2FP%3E%0A%3CP%3E%3CFONT%20size%3D%222%22%3EThis%20is%20a%20new%20JEDEC%20100%20ball%20package%2C%20half%20the%20size%20of%20the%20standard%20200%20ball%20package.%20This%20100%20ball%20package%20has%20the%20same%20performance%20and%20functionality%20as%20the%20200%20ball%20package%2C%20and%20has%20the%20added%20advantage%20of%20being%20smaller%20and%20cheaper%20than%20the%20standard%20package.%3C%2FFONT%3E%3C%2FP%3E%0A%3CP%3E%3CSTRONG%3ENote%207%3A%3C%2FSTRONG%3E%3C%2FP%3E%0A%3CP%3E%3CFONT%20size%3D%222%22%3EThis%20device%20has%20been%20EoLed%20by%20the%20manufacturer%20and%20has%20been%20updated%20by%20a%20new%20memory%20part%20number%26nbsp%3B%3C%2FFONT%3E%3C%2FP%3E%0A%3CP%3E%3CFONT%20size%3D%222%22%3E%3CFONT%20size%3D%223%22%3E%3CSTRONG%3ENote%208%3A%3C%2FSTRONG%3E%3C%2FFONT%3E%3C%2FFONT%3E%3C%2FP%3E%0A%3CP%3E%3CFONT%20size%3D%222%22%3EPart%20is%20active.%20Reviewed%20Q3%202026%3C%2FFONT%3E%3C%2FP%3E%0A%3CP%3E%3CFONT%20size%3D%222%22%3E%3CFONT%20size%3D%223%22%3E%3CSTRONG%3ENote%209%3A%3C%2FSTRONG%3E%3C%2FFONT%3E%3C%2FFONT%3E%3C%2FP%3E%0A%3CP%3E%3CFONT%20size%3D%222%22%3EPart%20is%20obsolete.%3C%2FFONT%3E%3C%2FP%3E%0A%3CP%3E%3CSTRONG%3ENote%2010%3A%3C%2FSTRONG%3E%3C%2FP%3E%0A%3CP%3E%3CFONT%20size%3D%222%22%3EThis%20device%20will%20be%20EoLed%20in%20Q2%2024%20by%20the%20manufacturer%20and%20will%20not%20be%20updated%20by%20a%20new%20memory%20part%20number%3C%2FFONT%3E%3C%2FP%3E%0A%3CP%3E%3CSTRONG%3ENote%2011%3A%3C%2FSTRONG%3E%3C%2FP%3E%0A%3CP%3E%3CFONT%20size%3D%222%22%3EDQ%20eye%20marginalities%20were%20identified%20during%20TSA%20analysis.%20vTSA%20and%20stability%20testing%20did%20not%20identify%20any%20issues.%3C%2FFONT%3E%3C%2FP%3E%0A%3C%2FLINGO-BODY%3E
100% helpful (8/8)
Version history
Last update:
a week ago
Updated by: