This document describes all the i.MX 8 MIPI-CSI use cases, showing the available cameras and daughter cards supported by the boards, the compatible Device Trees (DTS) files, and how to enable these different camera options on the i.MX 8 boards.
Plus, this document describes some Advanced camera use cases too, such as multiples cameras output using imxcompositor_g2d plugin, GStreamer zero-copy pipelines and V4L2 API extra-controls examples.
Hi,
Thanks for posting this guide. It would be nice to add hardware accelerated JPEG encoding and decoding examples for i.MX8QXP/i.MX8QM
Hi Ofer,
Thanks for your suggestion. But I believe it fits better at the GStreamer doc below:
https://community.nxp.com/docs/DOC-347107
I will include it in the v2.0 release.
BR,
Marco
Hi Marco,
Great work!
In your example 3.3 MCIMXCAMERA1MP camera daughter card, you have four cameras connected to the daughter card.
Thanks again!
SPA
Hi Sebster,
I am glad you like it.
Regarding your questions, the i.MX 8QXP and i.MX 8QM has independent MIPI-CSI channel interfaces, so you can get the max camera resolution on each channel. But of course, there will be some bandwidth limitations to be considered as well.
Regarding the VPU, unfortunately, I do not have any doc about it, but it is a great test to be done.
It would be great if you opened a community thread to check these topics. I am sure it will help a lot of people.
Best Regards,
Marco
Are there any documents describing control of MIPI and receiving images on a lower level?
According to the "use cases" manual "This camera will be allocated on /dev/video0". And the mentioned example (gst-launch1.0 v4l2src device=/dev/video0 ! autovideosink) works - it mirrors the camera input to HDMI.
But: If I want to grab from that camera with examples as : linux/v4l2 – Gateworks I get the message:
./capture /dev/video0 1920 1080 1
VIDIOC_G_STD: Inappropriate ioctl for device
VIDIOC_S_STD: Inappropriate ioctl for device
found NTSC TV decoder
found SECAM TV decoder
found PAL TV decoder
/dev/video0 is no video capture device
Why this is not a capture device ???
This is result of
v4l2-ctl --all -d /dev/video0
Driver Info:
Driver name : mxc-isi-cap
Card type : mxc-isi-cap
Bus info : platform:32e00000.isi:cap_devic
Driver version : 5.4.24
Capabilities : 0x84201000
Video Capture Multiplanar
Streaming
Extended Pix Format
Device Capabilities
Device Caps : 0x04201000
Video Capture Multiplanar
Streaming
Extended Pix Format
Media Driver Info:
Driver name : mxc-md
Model : FSL Capture Media Device
Serial :
Bus info :
Media version : 5.4.24
Hardware revision: 0x00000000 (0)
Driver version : 5.4.24
Interface Info:
ID : 0x03000014
Type : V4L Video
Entity Info:
ID : 0x00000012 (18)
Name : mxc_isi.0.capture
Function : V4L2 I/O
Pad 0x01000013 : 0: Sink
Link 0x02000021: from remote pad 0x100000e of entity 'mxc_isi.0': Data, Enabled
Priority: 2
Format Video Capture Multiplanar:
Width/Height : 0/0
Pixel Format : 'RGBP' (16-bit RGB 5-6-5)
Field : None
Number of planes : 1
Flags :
Colorspace : JPEG
Transfer Function : Default
YCbCr/HSV Encoding: Default
Quantization : Default
Plane 0 :
Bytes per Line : 0
Size Image : 0
Streaming Parameters Video Capture:
Capabilities : timeperframe
Frames per second: 30.000 (30/1)
Read buffers : 0
User Controls
horizontal_flip 0x00980914 (bool) : default=0 value=0
vertical_flip 0x00980915 (bool) : default=0 value=0
alpha_component 0x00980929 (int) : min=0 max=255 step=1 default=0 value=0