Hi all,
I'm trying to port Android JB to a custom board based on imx6q.
I'm not able to get the launcher. And even the display is shifting to right. The kernel i've tested with linux where the display is proper.
Below is log.
In the log Marked are the issues I'm facing.
Any advice is helpful.
I'm in very critical stage. Please help me to resolve this. I'm the source from android_jb4.2.2_1.0.0-ga_source bundle package.
Uncompressing Linux... done, booting the kernel.
Initializing cgroup subsys cpu
Linux version 3.0.35-gcbaa4e0-dirty (rangam@PHYTECIndia) (gcc version 4.4.1 (Sourcery G++ Lite 2009q3-67) ) #11 SMP PREEMPT Fri Jul 26 16:57:13 IST 2013
CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d
CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine: Phytec
Memory policy: ECC disabled, Data cache writealloc
CPU identified as i.MX6Q, silicon rev 1.2
PERCPU: Embedded 7 pages/cpu @c13ec000 s6592 r8192 d13888 u32768
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 215040
Kernel command line: console=ttymxc3,115200 androidboot.hardware=freescale androidboot.console=ttymxc3 init=/init vmalloc=256M video=mxcfb1:dev=ldb,Primeview-PM070WL4,bpp
=16 fbmem=10M vt.global_cursor_default=0 consoleblank=0 board_mx6q_phyflex.csi0=none board_mx6q_phyflex.csi1=none video=mxcfb1:off video=mxcfb2:off ip=none root=/dev/mmcbl
k0p2 rootfstype=ext4 noinitrd rootwait mtdparts=n25q128:512k(barebox)ro,128k(bareboxenv),2M(splash),-(kernel);gpmi-nand:512k(barebox)ro,128k(bareboxenv),2M(splash),8M(kern
el),-(root)
PID hash table entries: 4096 (order: 2, 16384 bytes)
Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
Memory: 592MB 256MB = 848MB total
Memory: 847036k/847036k available, 201540k reserved, 311296K highmem
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
DMA : 0xfbe00000 - 0xffe00000 ( 64 MB)
vmalloc : 0xe2800000 - 0xf2000000 ( 248 MB)
lowmem : 0xc0000000 - 0xe2000000 ( 544 MB)
pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
.init : 0xc0008000 - 0xc0047000 ( 252 kB)
.text : 0xc0047000 - 0xc09dbebc (9812 kB)
.data : 0xc09dc000 - 0xc0a59f18 ( 504 kB)
.bss : 0xc0a59f3c - 0xc0be2d40 (1572 kB)
Preemptible hierarchical RCU implementation.
NR_IRQS:624
MXC GPIO hardware
sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655ms
arm_max_freq=1GHz
MXC_Early serial console at MMIO 0x21f0000 (options '115200')
bootconsole [ttymxc3] enabled
Console: colour dummy device 80x30
Calibrating delay loop... 789.70 BogoMIPS (lpj=3948544)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 512
Initializing cgroup subsys debug
Initializing cgroup subsys cpuacct
Initializing cgroup subsys freezer
CPU: Testing write buffer coherency: ok
hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available
CPU1: Booted secondary processor
CPU2: Booted secondary processor
CPU3: Booted secondary processor
Brought up 4 CPUs
SMP: Total of 4 processors activated (3158.83 BogoMIPS).
devtmpfs: initialized
print_constraints: dummy:
NET: Registered protocol family 16
print_constraints: vddpu: 725 <--> 1300 mV at 1100 mV fast normal
print_constraints: vddcore: 725 <--> 1300 mV at 1100 mV fast normal
print_constraints: vddsoc: 725 <--> 1300 mV at 1100 mV fast normal
print_constraints: vdd2p5: 2000 <--> 2775 mV at 2400 mV fast normal
print_constraints: vdd1p1: 800 <--> 1400 mV at 1100 mV fast normal
print_constraints: vdd3p0: 2625 <--> 3400 mV at 3000 mV fast normal
imx_add_mxc_pwm:pdata= (null)
imx_add_mxc_pwm:pdata= (null)
imx_add_mxc_pwm:pdata= (null)
imx_add_mxc_pwm:pdata= (null)
hw-breakpoint: found 6 breakpoint and 1 watchpoint registers.
hw-breakpoint: 1 breakpoint(s) reserved for watchpoint single-step.
hw-breakpoint: maximum watchpoint size is 4 bytes.
L310 cache controller enabled
l2x0: 16 ways, CACHE_ID 0x410000c7, AUX_CTRL 0x02070000, Cache size: 1048576 B
bio: create slab <bio-0> at 0
mxs-dma mxs-dma-apbh: initialized
print_constraints: vmmc: 3300 mV
print_constraints: IOVDD: 3300 mV
print_constraints: DVDD: 1800 mV
print_constraints: AVDD: 3300 mV
print_constraints: DRVDD: 3300 mV
vgaarb: loaded
i2c-core: driver [da9063] using legacy suspend method
i2c-core: driver [da9063] using legacy resume method
SCSI subsystem initialized
spi_imx imx6q-ecspi.2: probed
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
Freescale USB OTG Driver loaded, $Revision: 1.55 $
i2c-gpio i2c-gpio.3: using pins 109 (SDA) and 108 (SCL)
print_constraints: VDDCORE: 730 <--> 1280 mV at 1300 mV at 2000 mA normal
print_constraints: VDDSOC: 730 <--> 1280 mV at 1300 mV at 500 mA normal
print_constraints: VDD_DDR3: 1500 mV at 2000 mA
print_constraints: VDD_3V3: 3300 mV at 1500 mA
print_constraints: VDD_BUCKMEM: 3300 mV at 1500 mA
print_constraints: VDD_ETH: 1200 mV at 3000 mA
print_constraints: VDD_ETH_IO: 3300 mV
print_constraints: VDD_MX6_SNVS: 3300 mV
print_constraints: VDD_3V3_PMIC_IO: 3300 mV
print_constraints: VDD_SD0: 3300 mV
print_constraints: VDD_SD1: 3300 mV
print_constraints: VDD_MX6_HIGH: 3000 mV
da9063 0-0058: Device detected DA9063
max7300: probe of 0-0040 failed with error -5
stmpe 1-0041: stmpe811 detected, chip id: 0x811
stmpe 2-0041: failed to read regs 0x0: -5
stmpe: probe of 2-0041 failed with error -5
imx-ipuv3 imx-ipuv3.0: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
imx-ipuv3 imx-ipuv3.1: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
Advanced Linux Sound Architecture Driver Version 1.0.24.
Bluetooth: Core ver 2.16
NET: Registered protocol family 31
Bluetooth: HCI device and connection manager initialized
Bluetooth: HCI socket layer initialized
Bluetooth: L2CAP socket layer initialized
Bluetooth: SCO socket layer initialized
cfg80211: Calling CRDA to update world regulatory domain
Switching to clocksource mxc_timer1
NET: Registered protocol family 2
IP route cache hash table entries: 32768 (order: 5, 131072 bytes)
TCP established hash table entries: 131072 (order: 8, 1048576 bytes)
TCP bind hash table entries: 65536 (order: 7, 786432 bytes)
TCP: Hash tables configured (established 131072 bind 65536)
TCP reno registered
UDP hash table entries: 512 (order: 2, 16384 bytes)
UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
Static Power Management for Freescale i.MX6
wait mode is enabled for i.MX6
cpaddr = e2880000 suspend_iram_base=e291c000
PM driver module loaded
link up failed, DB_R0:0x00913b00, DB_R1:0x08200000!
IMX PCIe port: link down with power supply 0!
IMX usb wakeup probe
add wake up source irq 75
IMX usb wakeup probe
cpu regulator mode:ldo_bypass
_regulator_get: get() with no identifier
mx6_cpu_regulator_init: failed to get pu regulator
i.MXC CPU frequency driver
highmem bounce pool size: 64 pages
ashmem: initialized
NTFS driver 2.1.30 [Flags: R/O].
JFFS2 version 2.2. (NAND) �© 2001-2006 Red Hat, Inc.
fuse init (API version 7.16)
msgmni has been set to 1046
NET: Registered protocol family 38
cryptodev: driver loaded.
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
mxc_sdc_fb mxc_sdc_fb.0: register mxc display driver ldb
_regulator_get: get() with no identifier
ldb_clk to di clk: ldb_di0_clk -> ipu1_di0_clk
mxc_sdc_fb mxc_sdc_fb.1: mxcfb1 is turned off!
imx-sdma imx-sdma: loaded firmware 1.1
imx-sdma imx-sdma: initialized
Serial: IMX driver
imx-uart.2: ttymxc2 at MMIO 0x21ec000 (irq = 60) is a IMX
imx-uart.3: ttymxc3 at MMIO 0x21f0000 (irq = 61) is a IMX
console [ttymxc3] enabled, bootconsole disabled
console [ttymxc3] enabled, bootconsole disabled
loop: module loaded
at24 0-0050: 4096 byte 24c32 EEPROM, writable, 8 bytes/write
at24 2-0052: 512 byte 24c04 EEPROM, writable, 16 bytes/write
No sata disk.
m25p80 spi2.0: unrecognized id n25q128
m25p80 spi2.0: unrecognized JEDEC id 20ba18
GPIO NAND driver, �© 2004 Simtec Electronics
NAND device: Manufacturer ID: 0xec, Chip ID: 0xd3 (Samsung NAND 1GiB 3,3V 8-bit)
5 cmdlinepart partitions found on MTD device gpmi-nand
Creating 5 MTD partitions on "gpmi-nand":
0x000000000000-0x000000080000 : "barebox"
0x000000080000-0x0000000a0000 : "bareboxenv"
0x0000000a0000-0x0000002a0000 : "splash"
0x0000002a0000-0x000000aa0000 : "kernel"
0x000000aa0000-0x000040000000 : "root"
GPMI NAND driver registered. (IMX)
vcan: Virtual CAN interface driver
CAN device driver interface
flexcan netdevice driver
flexcan imx6q-flexcan.0: device registered (reg_base=e29b0000, irq=142)
FEC Ethernet Driver
fec_enet_mii_bus: probed
PPP generic driver version 2.4.2
PPP Deflate Compression module registered
PPP BSD Compression module registered
PPP MPPE Compression module registered
NET: Registered protocol family 24
PPTP driver version 0.8.5
tun: Universal TUN/TAP device driver, 1.6
tun: (C) 1999-2004 Max Krasnyansky <maxk@qualcomm.com>
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
fsl-ehci fsl-ehci.0: Freescale On-Chip EHCI Host Controller
fsl-ehci fsl-ehci.0: new USB bus registered, assigned bus number 1
fsl-ehci fsl-ehci.0: irq 75, io base 0x02184000
fsl-ehci fsl-ehci.0: USB 2.0 started, EHCI 1.00
usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb1: Product: Freescale On-Chip EHCI Host Controller
usb usb1: Manufacturer: Linux 3.0.35-gcbaa4e0-dirty ehci_hcd
usb usb1: SerialNumber: fsl-ehci.0
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
add wake up source irq 72
fsl-ehci fsl-ehci.1: Freescale On-Chip EHCI Host Controller
fsl-ehci fsl-ehci.1: new USB bus registered, assigned bus number 2
fsl-ehci fsl-ehci.1: irq 72, io base 0x02184200
fsl-ehci fsl-ehci.1: USB 2.0 started, EHCI 1.00
usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb2: Product: Freescale On-Chip EHCI Host Controller
usb usb2: Manufacturer: Linux 3.0.35-gcbaa4e0-dirty ehci_hcd
usb usb2: SerialNumber: fsl-ehci.1
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 1 port detected
usbcore: registered new interface driver cdc_acm
cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
ARC USBOTG Device Controller driver (1 August 2005)
android_usb gadget: Mass Storage Function, version: 2009/09/11
android_usb gadget: Number of LUNs=1
lun0: LUN: removable file: (no medium)
Gadget Android: controller 'fsl-usb2-udc' not recognized
android_usb gadget: android_usb ready
Suspend udc for OTG auto detect
fsl-usb2-udc: bind to driver android_usb
mousedev: PS/2 mouse device common for all mice
input: stmpe-ts as /devices/virtual/input/input0
i2c-core: driver [isl29023] using legacy suspend method
i2c-core: driver [isl29023] using legacy resume method
using rtc device, da9063-rtc, for alarms
da9063-rtc da9063-rtc: rtc core: registered da9063-rtc as rtc0
da9063-rtc da9063-rtc: Failed to request ALARM IRQ.
rtc-pcf8563 1-0051: chip found, driver version 0.4.3
rtc-pcf8563 1-0051: rtc core: registered rtc-pcf8563 as rtc1
snvs_rtc snvs_rtc.0: rtc core: registered snvs_rtc as rtc2
i2c /dev entries driver
Linux video capture interface: v2.00
mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video16
mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video17
usbcore: registered new interface driver uvcvideo
USB Video Class driver (v1.1.0)
Driver for 1-wire Dallas network protocol.
i2c-core: driver [mag3110] using legacy suspend method
i2c-core: driver [mag3110] using legacy resume method
imx2-wdt imx2-wdt.0: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=1)
Bluetooth: HCI UART driver ver 2.2
Bluetooth: HCILL protocol initialized
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
mmc0: SDHCI controller on platform [sdhci-esdhc-imx.2] using DMA
w1_master_driver w1 bus master: Family 43 for 43.000000436e56.c7 is not registered.
mmc1: SDHCI controller on platform [sdhci-esdhc-imx.1] using DMA
VPU initialized
mxc_asrc registered
revserved_memory_account:viv_gpu registerd
Thermal calibration data is 0x5914c97d
Thermal sensor with ratio = 185
w1_master_driver w1 bus master: Family 43 for 43.0000003be6e7.b6 is not registered.
Anatop Thermal registered as thermal_zone0
anatop_thermal_probe: default cooling device is cpufreq!
HDMI CEC initialized
leds-pca953x 1-0062: setting platform data
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
usb 2-1: new high speed USB device number 2 using fsl-ehci
logger: created 256K log 'log_main'
logger: created 256K log 'log_events'
logger: created 256K log 'log_radio'
logger: created 256K log 'log_system'
usbcore: registered new interface driver snd-usb-audio
mxc_hdmi_soc mxc_hdmi_soc.0: MXC HDMI Audio
imx-hdmi-soc-dai imx-hdmi-soc-dai.0: Failed: Load HDMI-video first.
tlv320aic3x-codec 1-0018: asoc: failed to add kcontrol Left Line1R Mux
tlv320aic3x-codec 1-0018: asoc: failed to add kcontrol Left Line1L Mux
asoc: tlv320aic3x-hifi <-> imx-ssi.1 mapping ok
Initialize HDMI-audio failed. Load HDMI-video first!
ALSA device list:
#0: imx_tlv320aic3007-audio
oprofile: using arm/armv7-ca9
GACT probability NOT on
Mirror/redirect action on
u32 classifier
Actions configured
Netfilter messages via NETLINK v0.30.
nf_conntrack version 0.5.0 (13234 buckets, 52936 max)
ctnetlink v0.93: registering with nfnetlink.
NF_TPROXY: Transparent proxy support initialized, version 4.1.0
NF_TPROXY: Copyright (c) 2006-2007 BalaBit IT Ltd.
xt_time: kernel timezone is -0000
IPv4 over IPv4 tunneling driver
GRE over IPv4 demultiplexor driver
ip_tables: (C) 2000-2006 Netfilter Core Team
arp_tables: (C) 2002 David S. Miller
TCP cubic registered
NET: Registered protocol family 10
Mobile IPv6
ip6_tables: (C) 2000-2006 Netfilter Core Team
IPv6 over IPv4 tunneling driver
NET: Registered protocol family 17
mmc0: new SD card at address e624
NET: Registered protocol family 15
can: controller area network core (rev 20090105 abi 8)
NET: Registered protocol family 29
mmcblk0: mmc0:e624 SU02G 1.84 GiB
mmcblk0: p1 p2 p3
can: raw protocol (rev 20090105)
can: broadcast manager protocol (rev 20090105 t)
Bluetooth: RFCOMM TTY layer initialized
Bluetooth: RFCOMM socket layer initialized
Bluetooth: RFCOMM ver 1.11
Bluetooth: BNEP (Ethernet Emulation) ver 1.3
Bluetooth: BNEP filters: protocol multicast
Bluetooth: HIDP (Human Interface Emulation) ver 1.2
L2TP core driver, V2.0
PPPoL2TP kernel driver, V2.0
L2TP IP encapsulation support (L2TPv3)
L2TP netlink interface
L2TP ethernet pseudowire support (L2TPv3)
lib80211: common routines for IEEE802.11 drivers
VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
Bus freq driver module loaded
Bus freq driver Enabled
mxc_dvfs_core_probe
usb 2-1: New USB device found, idVendor=0451, idProduct=8042
usb 2-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
hub 2-1:1.0: USB hub found
hub 2-1:1.0: 4 ports detected
DVFS driver module loaded
regulator_init_complete: VDD_MX6_HIGH: incomplete constraints, leaving on
regulator_init_complete: VDD_SD1: incomplete constraints, leaving on
regulator_init_complete: VDD_SD0: incomplete constraints, leaving on
regulator_init_complete: VDD_3V3_PMIC_IO: incomplete constraints, leaving on
regulator_init_complete: VDD_MX6_SNVS: incomplete constraints, leaving on
regulator_init_complete: VDD_ETH_IO: incomplete constraints, leaving on
regulator_init_complete: VDD_ETH: incomplete constraints, leaving on
regulator_init_complete: VDD_3V3: incomplete constraints, leaving on
regulator_init_complete: VDD_DDR3: incomplete constraints, leaving on
regulator_init_complete: VDDSOC: incomplete constraints, leaving on
regulator_init_complete: VDDCORE: incomplete constraints, leaving on
regulator_init_complete: DRVDD: incomplete constraints, leaving on
regulator_init_complete: AVDD: incomplete constraints, leaving on
regulator_init_complete: DVDD: incomplete constraints, leaving on
regulator_init_complete: IOVDD: incomplete constraints, leaving on
da9063-rtc da9063-rtc: setting system clock to 2000-01-01 00:01:34 UTC (946684894)
EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
VFS: Mounted root (ext4 filesystem) on device 179:2.
devtmpfs: mounted
Freeing init memory: 252K
init (1): /proc/1/oom_adj is deprecated, please use /proc/1/oom_score_adj instead.
init: cannot open '/initlogo.rle'
EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
init: Unable to open persistent property directory /data/property errno: 2
init: using deprecated syntax for specifying property 'ro.product.manufacturer', use ${name} instead
init: using deprecated syntax for specifying property 'ro.product.model', use ${name} instead
init: using deprecated syntax for specifying property 'ro.serialno', use ${name} instead
init: cannot find '/system/etc/install-recovery.sh', disabling 'flash_recovery'
android_usb: already disabled
android_usb: already disabled
mtp_bind_config
root@android:/ # request_suspend_state: wakeup (3->0) at 8290682004 (2000-01-01 00:01:39.585311336 UTC)
init: untracked pid 2494 exited
request_suspend_state: wakeup (0->0) at 8890367671 (2000-01-01 00:01:40.184997336 UTC)
init: untracked pid 2543 exited
root@android:/ #
root@android:/ #
root@android:/ #
root@android:/ #
root@android:/ #
root@android:/ # lrequest_suspend_state: wakeup (0->0) at 14500371003 (2000-01-01 00:01:45.795000669 UTC)
init: untracked pid 2551 exited
root@android:/ # logcat
--------- beginning of /dev/log/main
I/installd( 2495): installd firing up
E/cutils ( 2495): Failed to read /data/.layout_version: No such file or directory
E/installd( 2495): Could not create directories; exiting.
--------- beginning of /dev/log/system
I/Vold ( 2489): Vold 2.1 (the revenge) firing up
D/Vold ( 2489): Volume udisk state changing -1 (Initializing) -> 0 (No-Media)
D/Vold ( 2489): Volume extsd state changing -1 (Initializing) -> 0 (No-Media)
D/Vold ( 2489): Volume sdcard state changing -1 (Initializing) -> 0 (No-Media)
D/Vold ( 2489): Volume sdcard state changing 0 (No-Media) -> 2 (Pending)
D/Vold ( 2489): Volume sdcard state changing 2 (Pending) -> 1 (Idle-Unmounted)
I/SurfaceFlinger( 2491): SurfaceFlinger is starting
I/SurfaceFlinger( 2491): SurfaceFlinger's main thread ready to run. Initializing graphics H/W...
D/libEGL ( 2491): loaded /system/lib/egl/libEGL_VIVANTE.so
D/libEGL ( 2491): loaded /system/lib/egl/libGLESv1_CM_VIVANTE.so
D/libEGL ( 2491): loaded /system/lib/egl/libGLESv2_VIVANTE.so
W/imx6.gralloc( 2491): using (fd=15)
W/imx6.gralloc( 2491): id = DISP3 BG
W/imx6.gralloc( 2491): xres = 800 px
W/imx6.gralloc( 2491): yres = 480 px
W/imx6.gralloc( 2491): xres_virtual = 800 px
W/imx6.gralloc( 2491): yres_virtual = 1536 px
W/imx6.gralloc( 2491): bpp = 16
W/imx6.gralloc( 2491): r = 11:5
W/imx6.gralloc( 2491): g = 5:6
W/imx6.gralloc( 2491): b = 0:5
W/imx6.gralloc( 2491): width = 127 mm (160.000000 dpi)
W/imx6.gralloc( 2491): height = 76 mm (160.421051 dpi)
W/imx6.gralloc( 2491): refresh rate = 35.70 Hz
I/FslHwcomposer( 2491): fb0 is ldb
I/FslHwcomposer( 2491): device
I/FslHwcomposer( 2491): fb1 is overlay device
W/FslHwcomposer( 2491): open /sys/class/graphics/fb2 failed
W/FslHwcomposer( 2491): open /sys/class/graphics/fb3 failed
W/FslHwcomposer( 2491): open /sys/class/graphics/fb4 failed
W/FslHwcomposer( 2491): open /sys/class/graphics/fb5 failed
I/FslHwcomposer( 2491): hwcomposer: open framebuffer fb0
I/v_hwc ( 2491): Detected display /dev/graphics/fb0
I/v_hwc ( 2491): xres = 800 px
I/v_hwc ( 2491): yres = 480 px
I/v_hwc ( 2491): xres_virtual = 800 px
I/v_hwc ( 2491): yres_virtual = 1536 px
I/v_hwc ( 2491): width = -1 mm (0.0 dpi)
I/v_hwc ( 2491): height = -1 mm (0.0 dpi)
I/v_hwc ( 2491): refresh rate = 35.0 Hz
E/v_hwc ( 2491): open /dev/graphics/fb0 failed
I/v_hwc ( 2491): Vivante HWComposer v2.4
I/v_hwc ( 2491): Device: 0x40039008
I/v_hwc ( 2491): Separated 2D: YES
I/v_hwc ( 2491): 2D PE20: YES
I/v_hwc ( 2491): Multi-source blit: NO
I/v_hwc ( 2491): Multi-source blit Ex: NO
I/v_hwc ( 2491): OPF/YUV blit/Tiling : NO
I/v_hwc ( 2491): Filter stretch : NO
I/FslHwcomposer( 2491): hwc_device_open,367
I/SurfaceFlinger( 2491): Using composer version 1.1
W/SurfaceFlinger( 2491): no suitable EGLConfig found, trying without EGL_FRAMEBUFFER_TARGET_ANDROID
E/Trace ( 2491): error opening trace file: No such file or directory (2)
E/SurfaceFlinger( 2491): HWComposer: framebufferTarget is null
E/SurfaceFlinger( 2491): HWComposer: framebufferTarget is null
E/SurfaceFlinger( 2491): HWComposer: framebufferTarget is null
E/SurfaceFlinger( 2491): HWComposer: framebufferTarget is null
I/SurfaceFlinger( 2491): EGL informations:
I/SurfaceFlinger( 2491): vendor : Android
I/SurfaceFlinger( 2491): version : 1.4 Android META-EGL
I/SurfaceFlinger( 2491): extensions: EGL_KHR_image EGL_KHR_image_base EGL_KHR_image_pixmap EGL_KHR_gl_texture_2D_image EGL_KHR_gl_renderbuffer_image EGL_KHR_fence_sync EGL
_ANDROID_image_native_buffer
I/SurfaceFlinger( 2491): Client API: OpenGL_ES
I/SurfaceFlinger( 2491): EGLSurface: 8-8-8-8, config=0x4b7d5138
I/SurfaceFlinger( 2491): OpenGL ES informations:
I/SurfaceFlinger( 2491): vendor : Vivante Corporation
I/SurfaceFlinger( 2491): renderer : GC2000 Graphics Engine
I/SurfaceFlinger( 2491): version : OpenGL ES-CM 1.1
I/SurfaceFlinger( 2491): extensions: GL_EXT_debug_marker GL_OES_blend_equation_separate GL_OES_blend_func_separate GL_OES_blend_subtract GL_OES_byte_coordinates GL_OES_com
pressed_ETC1_RGB8_texture GL_OES_compressed_paletted_texture GL_OES_draw_texture GL_OES_extended_matrix_palette GL_OES_fixed_point GL_OES_framebuffer_object GL_OES_matrix_
get GL_OES_matrix_palette GL_OES_point_size_array GL_OES_point_sprite GL_OES_query_matrix GL_OES_read_format GL_OES_single_precision GL_OES_stencil_wrap GL_OES_texture_cub
e_map GL_OES_texture_mirrored_repeat GL_OES_EGL_image GL_OES_depth24 GL_OES_element_index_uint GL_OES_fbo_render_mipmap GL_OES_mapbuffer GL_OES_rgb8_rgba8 GL_OES_stencil1
GL_OES_stencil4 GL_OES_stencil8 GL_OES_texture_npot GL_OES_vertex_half_float GL_OES_packed_depth_stencil GL_EXT_texture_format_BGRA8888 GL_IMG_read_format GL_IMG_user_clip
_plane GL_APPLE_texture_2D_limited_npot GL_EXT_texture_lod_bias GL_EXT_blend_minmax GL_EXT_read_format_bgra GL_EXT_multi_draw_arrays GL_OES_EGL_sync GL_APPLE_texture_forma
t_BGRA8888 GL_APPLE_te
I/SurfaceFlinger( 2491): GL_MAX_TEXTURE_SIZE = 8192
I/SurfaceFlinger( 2491): GL_MAX_VIEWPORT_DIMS = 8192 x 8192
D/AndroidRuntime( 2492):
D/AndroidRuntime( 2492): >>>>>> AndroidRuntime START com.android.internal.os.ZygoteInit <<<<<<
D/AndroidRuntime( 2492): CheckJNI is OFF
I/AndroidRuntime( 2492): JNI options: '-Xjniopts:warnonly'
D/SurfaceFlinger( 2491): Screen acquired, type=0 flinger=0x404f0318
D/libEGL ( 2531): loaded /system/lib/egl/libEGL_VIVANTE.so
D/libEGL ( 2531): loaded /system/lib/egl/libGLESv1_CM_VIVANTE.so
D/libEGL ( 2531): loaded /system/lib/egl/libGLESv2_VIVANTE.so
E/Trace ( 2531): error opening trace file: No such file or directory (2)
E/BufferQueue( 2491): [BootAnimation] dequeueBuffer: can't dequeue multiple buffers without setting the buffer count
I/mediaserver( 2494): ServiceManager: 0x40a56ef8
I/AudioFlinger( 2494): Using default 3000 mSec as standby time.
I/CameraService( 2494): CameraService started (pid=2494)
I/v_hwc ( 2491): Display(0x4010c008) detected: format=306 800x480
I/v_hwc ( 2491): Display buffer(0x40050de0) detected: physical=0x2f800000
I/v_hwc ( 2491): Display buffer(0x40050e08) detected: physical=0x2f8bb800
I/FslCameraHAL( 2494): Face Back Camera is ov5642, orient is 0
I/FslCameraHAL( 2494): Face Front Camera is 0, orient is 0
I/FslCameraHAL( 2494): Camera ID 0: name ov5642, Facing 0, orientation 0, dev path
I/v_hwc ( 2491): Display buffer(0x400d57a8) detected: physical=0x2f977000
I/AudioPolicyManagerBase( 2494): loadAudioPolicyConfig() loaded /system/etc/audio_policy.conf
W/audio_hw_primary( 2494): card 0, id imxtlv320aic300 ,driver imx_tlv320aic30, name imx_tlv320aic3007-audio
W/audio_hw_primary( 2494): out rate 44100
W/audio_hw_primary( 2494): in rate 44100, channels 1 format 0
I/AudioFlinger( 2494): loadHwModule() Loaded primary audio interface from Freescale i.MX Audio HW HAL (audio) handle 1
W/audio_hw_primary( 2494): open output stream devices 2, format 1, channels 3, sample_rate 48000, flag 2
W/audio_hw_primary( 2494): opened out stream...1086925552
I/AudioFlinger( 2494): HAL output buffer size 192 frames, normal mix buffer size 768 frames
I/AudioMixer( 2494): found effect "Multichannel Downmix To Stereo" from The Android Open Source Project
E/MonoPipe( 2494): Failed to fetch local time frequency when constructing a MonoPipe (res = -32). getNextWriteTimestamp calls will be non-functional
D/dalvikvm( 2492): Trying to load lib libjavacore.so 0x0
D/dalvikvm( 2492): Added shared lib libjavacore.so 0x0
D/dalvikvm( 2492): Trying to load lib libnativehelper.so 0x0
D/dalvikvm( 2492): Added shared lib libnativehelper.so 0x0
I/SamplingProfilerIntegration( 2492): Profiling disabled.
I/Zygote ( 2492): Preloading classes...
D/dalvikvm( 2492): GC_EXPLICIT freed 36K, 9% free 419K/460K, paused 1ms+0ms, total 3ms
W/Environment( 2492): EXTERNAL_STORAGE undefined; falling back to default
W/dalvikvm( 2492): Exception Ljava/lang/NullPointerException; thrown while initializing Landroid/os/Debug;
D/AndroidRuntime( 2492): Shutting down VM
W/dalvikvm( 2492): threadid=1: thread exiting with uncaught exception (group=0x4143c930)
I/installd( 2542): installd firing up
E/cutils ( 2542): Failed to read /data/.layout_version: No such file or directory
E/installd( 2542): Could not create directories; exiting.
I/ServiceManager( 2488): service 'media.camera' died
I/ServiceManager( 2488): service 'media.audio_flinger' died
I/ServiceManager( 2488): service 'media.player' died
D/AndroidRuntime( 2544):
D/AndroidRuntime( 2544): >>>>>> AndroidRuntime START com.android.internal.os.ZygoteInit <<<<<<
D/AndroidRuntime( 2544): CheckJNI is OFF
I/AndroidRuntime( 2544): JNI options: '-Xjniopts:warnonly'
D/dalvikvm( 2544): Trying to load lib libjavacore.so 0x0
D/dalvikvm( 2544): Added shared lib libjavacore.so 0x0
D/dalvikvm( 2544): Trying to load lib libnativehelper.so 0x0
D/dalvikvm( 2544): Added shared lib libnativehelper.so 0x0
I/mediaserver( 2543): ServiceManager: 0x40a68ef8
I/AudioFlinger( 2543): Using default 3000 mSec as standby time.
I/CameraService( 2543): CameraService started (pid=2543)
I/FslCameraHAL( 2543): Face Back Camera is ov5642, orient is 0
I/FslCameraHAL( 2543): Face Front Camera is 0, orient is 0
I/FslCameraHAL( 2543): Camera ID 0: name ov5642, Facing 0, orientation 0, dev path
I/AudioPolicyManagerBase( 2543): loadAudioPolicyConfig() loaded /system/etc/audio_policy.conf
W/audio_hw_primary( 2543): card 0, id imxtlv320aic300 ,driver imx_tlv320aic30, name imx_tlv320aic3007-audio
W/audio_hw_primary( 2543): out rate 44100
W/audio_hw_primary( 2543): in rate 44100, channels 1 format 0
I/AudioFlinger( 2543): loadHwModule() Loaded primary audio interface from Freescale i.MX Audio HW HAL (audio) handle 1
W/audio_hw_primary( 2543): open output stream devices 2, format 1, channels 3, sample_rate 48000, flag 2
W/audio_hw_primary( 2543): opened out stream...1086774000
I/AudioFlinger( 2543): HAL output buffer size 192 frames, normal mix buffer size 768 frames
I/AudioMixer( 2543): found effect "Multichannel Downmix To Stereo" from The Android Open Source Project
E/MonoPipe( 2543): Failed to fetch local time frequency when constructing a MonoPipe (res = -32). getNextWriteTimestamp calls will be non-functional
I/SamplingProfilerIntegration( 2544): Profiling disabled.
I/Zygote ( 2544): Preloading classes...
D/dalvikvm( 2544): GC_EXPLICIT freed 36K, 9% free 419K/460K, paused 1ms+0ms, total 3ms
W/Environment( 2544): EXTERNAL_STORAGE undefined; falling back to default
W/dalvikvm( 2544): Exception Ljava/lang/NullPointerException; thrown while initializing Landroid/os/Debug;
D/AndroidRuntime( 2544): Shutting down VM
W/dalvikvm( 2544): threadid=1: thread exiting with uncaught exception (group=0x40b1a930)
I/ServiceManager( 2488): service 'media.camera' died
I/ServiceManager( 2488): service 'media.audio_flinger' died
I/ServiceManager( 2488): service 'media.player' died
I/mediaserver( 2551): ServiceManager: 0x41f7b000
I/AudioFlinger( 2551): Using default 3000 mSec as standby time.
I/CameraService( 2551): CameraService started (pid=2551)
I/FslCameraHAL( 2551): Face Back Camera is ov5642, orient is 0
I/FslCameraHAL( 2551): Face Front Camera is 0, orient is 0
I/FslCameraHAL( 2551): Camera ID 0: name ov5642, Facing 0, orientation 0, dev path
I/AudioPolicyManagerBase( 2551): loadAudioPolicyConfig() loaded /system/etc/audio_policy.conf
W/audio_hw_primary( 2551): card 0, id imxtlv320aic300 ,driver imx_tlv320aic30, name imx_tlv320aic3007-audio
W/audio_hw_primary( 2551): out rate 44100
W/audio_hw_primary( 2551): in rate 44100, channels 1 format 0
I/AudioFlinger( 2551): loadHwModule() Loaded primary audio interface from Freescale i.MX Audio HW HAL (audio) handle 1
W/audio_hw_primary( 2551): open output stream devices 2, format 1, channels 3, sample_rate 48000, flag 2
W/audio_hw_primary( 2551): opened out stream...1106785632
I/AudioFlinger( 2551): HAL output buffer size 192 frames, normal mix buffer size 768 frames
I/AudioMixer( 2551): found effect "Multichannel Downmix To Stereo" from The Android Open Source Project
E/MonoPipe( 2551): Failed to fetch local time frequency when constructing a MonoPipe (res = -32). getNextWriteTimestamp calls will be non-functional
I/installd( 2562): installd firing up
E/cutils ( 2562): Failed to read /data/.layout_version: No such file or directory
E/installd( 2562): Could not create directories; exiting.
D/AndroidRuntime( 2561):
D/AndroidRuntime( 2561): >>>>>> AndroidRuntime START com.android.internal.os.ZygoteInit <<<<<<
D/AndroidRuntime( 2561): CheckJNI is OFF
I/AndroidRuntime( 2561): JNI options: '-Xjniopts:warnonly'
D/dalvikvm( 2561): Trying to load lib libjavacore.so 0x0
D/dalvikvm( 2561): Added shared lib libjavacore.so 0x0
D/dalvikvm( 2561): Trying to load lib libnativehelper.so 0x0
D/dalvikvm( 2561): Added shared lib libnativehelper.so 0x0
I/SamplingProfilerIntegration( 2561): Profiling disabled.
I/Zygote ( 2561): Preloading classes...
D/dalvikvm( 2561): GC_EXPLICIT freed 36K, 9% free 419K/460K, paused 0ms+1ms, total 3ms
W/Environment( 2561): EXTERNAL_STORAGE undefined; falling back to default
W/dalvikvm( 2561): Exception Ljava/lang/NullPointerException; thrown while initializing Landroid/os/Debug;
D/AndroidRuntime( 2561): Shutting down VM
W/dalvikvm( 2561): threadid=1: thread exiting with uncaught exception (group=0x4200b930)
I/ServiceManager( 2488): service 'media.audio_flinger' died
I/ServiceManager( 2488): service 'media.player' died
I/ServiceManager( 2488): service 'media.camera' died
I/mediaserver( 2566): ServiceManager: 0x417df000
I/AudioFlinger( 2566): Using default 3000 mSec as standby time.
I/CameraService( 2566): CameraService started (pid=2566)
I/FslCameraHAL( 2566): Face Back Camera is ov5642, orient is 0
I/FslCameraHAL( 2566): Face Front Camera is 0, orient is 0
I/FslCameraHAL( 2566): Camera ID 0: name ov5642, Facing 0, orientation 0, dev path
I/AudioPolicyManagerBase( 2566): loadAudioPolicyConfig() loaded /system/etc/audio_policy.conf
W/audio_hw_primary( 2566): card 0, id imxtlv320aic300 ,driver imx_tlv320aic30, name imx_tlv320aic3007-audio
W/audio_hw_primary( 2566): out rate 44100
W/audio_hw_primary( 2566): in rate 44100, channels 1 format 0
I/AudioFlinger( 2566): loadHwModule() Loaded primary audio interface from Freescale i.MX Audio HW HAL (audio) handle 1
W/audio_hw_primary( 2566): open output stream drequest_suspend_state: wakeup (0->0) at 19200353004 (2000-01-01 00:01:50.494982670 UTC)
evices 2, format 1, channels 3, sinit: untracked pid 2566 exited
ample_rate 48000, flag 2
W/audio_hw_primary( 2566): opened out stream...1098806624
I/AudioFlinger( 2566): HAL output buffer size 192 frames, normal mix buffer size 768 frames
I/AudioMixer( 2566): found effect "Multichannel Downmix To Stereo" from The Android Open Source Project
E/MonoPipe( 2566): Failed to fetch local time frequency when constructing a MonoPipe (res = -32). getNextWriteTimestamp calls will be non-functional
I/v_hwc ( 2491): vsync thread exit: callback procs not registered.
I/installd( 2572): installd firing up
E/cutils ( 2572): Failed to read /data/.layout_version: No such file or directory
E/installd( 2572): Could not create directories; exiting.
D/AndroidRuntime( 2571):
D/AndroidRuntime( 2571): >>>>>> AndroidRuntime START com.android.internal.os.ZygoteInit <<<<<<
D/AndroidRuntime( 2571): CheckJNI is OFF
I/AndroidRuntime( 2571): JNI options: '-Xjniopts:warnonly'
D/dalvikvm( 2571): Trying to load lib libjavacore.so 0x0
D/dalvikvm( 2571): Added shared lib libjavacore.so 0x0
D/dalvikvm( 2571): Trying to load lib libnativehelper.so 0x0
D/dalvikvm( 2571): Added shared lib libnativehelper.so 0x0
I/SamplingProfilerIntegration( 2571): Profiling disabled.
I/Zygote ( 2571): Preloading classes...
D/dalvikvm( 2571): GC_EXPLICIT freed 36K, 9% free 419K/460K, paused 0ms+0ms, total 2ms
W/Environment( 2571): EXTERNAL_STORAGE undefined; falling back to default
W/dalvikvm( 2571): Exception Ljava/lang/NullPointerException; thrown while initializing Landroid/os/Debug;
D/AndroidRuntime( 2571): Shutting down VM
W/dalvikvm( 2571): threadid=1: thread exiting with uncaught exception (group=0x412e5930)
I/ServiceManager( 2488): service 'media.audio_flinger' died
I/ServiceManager( 2488): service 'media.player' died
I/ServiceManager( 2488): service 'media.camera' died
I/mediaserver( 2576): ServiceManager: 0x41724000
I/AudioFlinger( 2576): Using default 3000 mSec as standby time.
I/CameraService( 2576): CameraService started (pid=2576)
I/FslCameraHAL( 2576): Face Back Camera is ov5642, orient is 0
I/FslCameraHAL( 2576): Face Front Camera is 0, orient is 0
I/FslCameraHAL( 2576): Camera ID 0: name ov5642, Facing 0, orientation 0, dev path
I/AudioPolicyManagerBase( 2576): loadAudioPolicyConfig() loaded /system/etc/audio_policy.conf
W/audio_hw_primary( 2576): card 0, id imxtlv320aic300 ,driver imx_tlv320aic30, name imx_tlv320aic3007-audio
W/audio_hw_primary( 2576): out rate 44100
W/audio_hw_primary( 2576): in rate 44100, channels 1 format 0
I/AudioFlinger( 2576): loadHwModule() Loaded primary audio interface from Freescale i.MX Audio HW HAL (audio) handle 1
W/audio_hw_primary( 2576): open output stream devices 2, format 1, channels 3, sample_rate 48000, flag 2
W/audio_hw_primary( 2576): opened out stream...1098040672
I/AudioFlinger( 2576): HAL output buffer size 192 frames, normal mix buffer size 768 frames
I/AudioMixer( 2576): found effect "Multichannel Downmix To Stereo" from The Android Open Source Project
E/MonoPipe( 2576): Failed to fetch local time frequency when constructing a MonoPipe (res = -32). getNextWriteTimestamp calls will be non-functional
I/installd( 2581): installd firing up
E/cutils ( 2581): Failed to read /data/.layout_version: No such file or directory
E/installd( 2581): Could not create directories; exiting.
D/AndroidRuntime( 2580):
D/AndroidRuntime( 2580): >>>>>> AndroidRuntime START com.android.internal.os.ZygoteInit <<<<<<
D/AndroidRuntime( 2580): CheckJNI is OFF
I/AndroidRuntime( 2580): JNI options: '-Xjniopts:warnonly'
D/dalvikvm( 2580): Trying to load lib libjavacore.so 0x0
D/dalvikvm( 2580): Added shared lib libjavacore.so 0x0
D/dalvikvm( 2580): Trying to load lib libnativehelper.so 0x0
D/dalvikvm( 2580): Added shared lib libnativehelper.so 0x0
I/SamplingProfilerIntegration( 2580): Profiling disabled.
I/Zygote ( 2580): Preloading classes...
D/dalvikvm( 2580): GC_EXPLICIT freed 36K, 9% free 419K/460K, paused 0ms+0ms, total 3ms
W/Environment( 2580): EXTERNAL_STORAGE undefined; falling back to default
W/dalvikvm( 2580): Exception Ljava/lang/NullPointerException; thrown while initializing Landroid/os/Debug;
D/AndroidRuntime( 2580): Shutting down VM
W/dalvikvm( 2580): threadid=1: thread exiting with uncaught exception (group=0x40e62930)
request_suspend_state: wakeup (0->0) at 23810412672 (2000-01-01 00:01:55.105042004 UTC)
I/ServiceManager( 2488): service init: untracked pid 2576 exited
'media.audio_flinger' died
I/ServiceManager( 2488): service 'media.player' died
I/ServiceManager( 2488): service 'media.camera' died
I/mediaserver( 2585): ServiceManager: 0x40bcdfb0
I/AudioFlinger( 2585): Using default 3000 mSec as standby time.
I/CameraService( 2585): CameraService started (pid=2585)
I/FslCameraHAL( 2585): Face Back Camera is ov5642, orient is 0
I/FslCameraHAL( 2585): Face Front Camera is 0, orient is 0
I/FslCameraHAL( 2585): Camera ID 0: name ov5642, Facing 0, orientation 0, dev path
I/AudioPolicyManagerBase( 2585): loadAudioPolicyConfig() loaded /system/etc/audio_policy.conf
W/audio_hw_primary( 2585): card 0, id imxtlv320aic300 ,driver imx_tlv320aic30, name imx_tlv320aic3007-audio
W/audio_hw_primary( 2585): out rate 44100
W/audio_hw_primary( 2585): in rate 44100, channels 1 format 0
I/AudioFlinger( 2585): loadHwModule() Loaded primary audio interface from Freescale i.MX Audio HW HAL (audio) handle 1
W/audio_hw_primary( 2585): open output stream devices 2, format 1, channels 3, sample_rate 48000, flag 2
W/audio_hw_primary( 2585): opened out stream...1074431624
I/AudioFlinger( 2585): HAL output buffer size 192 frames, normal mix buffer size 768 frames
I/AudioMixer( 2585): found effect "Multichannel Downmix To Stereo" from The Android Open Source Project
E/MonoPipe( 2585): Failed to fetch local time frequency when constructing a MonoPipe (res = -32). getNextWriteTimestamp calls will be non-functional
I/installd( 2590): installd firing up
E/cutils ( 2590): Failed to read /data/.layout_version: No such file or directory
E/installd( 2590): Could not create directories; exiting.
D/AndroidRuntime( 2589):
D/AndroidRuntime( 2589): >>>>>> AndroidRuntime START com.android.internal.os.ZygoteInit <<<<<<
D/AndroidRuntime( 2589): CheckJNI is OFF
I/AndroidRuntime( 2589): JNI options: '-Xjniopts:warnonly'
D/dalvikvm( 2589): Trying to load lib libjavacore.so 0x0
D/dalvikvm( 2589): Added shared lib libjavacore.so 0x0
D/dalvikvm( 2589): Trying to load lib libnativehelper.so 0x0
D/dalvikvm( 2589): Added shared lib libnativehelper.so 0x0
I/SamplingProfilerIntegration( 2589): Profiling disabled.
I/Zygote ( 2589): Preloading classes...
D/dalvikvm( 2589): GC_EXPLICIT freed 36K, 9% free 419K/460K, paused 0ms+1ms, total 3ms
W/Environment( 2589): EXTERNAL_STORAGE undefined; falling back to default
W/dalvikvm( 2589): Exception Ljava/lang/NullPointerException; thrown while initializing Landroid/os/Debug;
D/AndroidRuntime( 2589): Shutting down VM
W/dalvikvm( 2589): threadid=1: thread exiting with uncaught exception (group=0x40ef1930)
request_suspend_state: wakeup (0->0) at 29440367339 (2000-01-01 00:02:00.734997005 UTC)
init: untracked pid 2585 exited
I/ServiceManager( 2488): service 'media.audio_flinger' died
I/ServiceManager( 2488): service 'media.player' died
I/ServiceManager( 2488): service 'media.camera' died
I/mediaserver( 2594): ServiceManager: 0x40b80fb0
I/AudioFlinger( 2594): Using default 3000 mSec as standby time.
I/CameraService( 2594): CameraService started (pid=2594)
I/FslCameraHAL( 2594): Face Back Camera is ov5642, orient is 0
I/FslCameraHAL( 2594): Face Front Camera is 0, orient is 0
I/FslCameraHAL( 2594): Camera ID 0: name ov5642, Facing 0, orientation 0, dev path
I/AudioPolicyManagerBase( 2594): loadAudioPolicyConfig() loaded /system/etc/audio_policy.conf
W/audio_hw_primary( 2594): card 0, id imxtlv320aic300 ,driver imx_tlv320aic30, name imx_tlv320aic3007-audio
W/audio_hw_primary( 2594): out rate 44100
W/audio_hw_primary( 2594): in rate 44100, channels 1 format 0
I/AudioFlinger( 2594): loadHwModule() Loaded primary audio interface from Freescale i.MX Audio HW HAL (audio) handle 1
W/audio_hw_primary( 2594): open output stream devices 2, format 1, channels 3, sample_rate 48000, flag 2
W/audio_hw_primary( 2594): opened out stream...1074105088
I/AudioFlinger( 2594): HAL output buffer size 192 frames, normal mix buffer size 768 frames
I/AudioMixer( 2594): found effect "Multichannel Downmix To Stereo" from The Android Open Source Project
E/MonoPipe( 2594): Failed to fetch local time frequency when constructing a MonoPipe (res = -32). getNextWriteTimestamp calls will be non-functional
The above issue is resolved now i'm able to get the home screen, but the display is divided in to 2, the actual left half shifted to right and actual right half shifted to left. and even the display color changed to dark yellow and the image latency is too low. I'll update with the images(screenshots) soon.
This document was generated from the following discussion: help in porting Android Jb to imx6q custom board
What should the permissions be? I have the following:
ueventd.freescale.rc:/dev/graphics/fb0 0660 system graphics
ueventd.freescale.rc:/sys/devices/platform/mxc_sdc_fb.0/graphics/fb* fsl_disp_property 0660 system graphics
ueventd.freescale.rc:/sys/devices/platform/mxc_sdc_fb.1/graphics/fb* fsl_disp_property 0660 system graphics
ueventd.freescale.rc:/sys/devices/platform/mxc_sdc_fb.0/graphics/fb* mode 0660 system graphics
ueventd.freescale.rc:/sys/devices/platform/mxc_sdc_fb.1/graphics/fb* mode 0660 system graphics
You need a SDcard. Debug.java is trying to create a trace file on it and can't open the sdcard path. Follow this guide and it'll be fine: Typical Configuration Examples | Android Developers