A new release of the manufacturing tool is was recently made available, "imx-3.10.53_1.1.0_ga-mfg-tools".
It can be found in the software download sections for the iMX6 family.
However, it can be used to program an iMX28 in a Win7 64-bit host by adding a few files.
The steps to do so are listed below and can be checked against the script in ucl2.xml.
- Download the attached "28.vbs" file and place it into where the manufacturing tool was installed, typically in <install_dir>\mfgtools\
- Replace <install_dir>\mfgtools\Profiles\Linux\OS Firmware\ucl2.xml with the attached ucl2.xml.
- Copy the attached files "updater_ivt.sb" and "fdisk-u.input" into <install_dir>\mfgtools\Profiles\Linux\OS Firmware\firmware
- Copy your iMX28 image file into <install_dir>\mfgtools\Profiles\Linux\OS Firmware\files. The file should be renamed to "linux.sb" to conform with the ucl2.xml script.
- Copy your "rootfs.tar.bz2" file into <install_dir>\mfgtools\Profiles\Linux\OS Firmware\files
To launch the manufacturing tool, double click on "28.vbs".
Issue:
After MfgTool has finished and the progress bars have turned green, clock on the Stop button or the program will start another cycle.