Transcode and Stream videos on i.MX6DLQ

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Transcode and Stream videos on i.MX6DLQ

Transcode and Stream videos on i.MX6DLQ

 

This article shows how to use the i.MX6DL/Q to transcode and stream videos on 1080i/p @ 24fps and 720p @ 30fps. For this test, we used one i.MX6DL as server and an i.MX6DL and i.MX6Q as clients. The video is streamed by the server, playing the sound at the same time, while the clients show the video in the HDMI output, as the image below:

 

Bio_TICFSL_0-1756400346080.jpeg

 

This test depends on some GStreamer plugins. To check that the right GStreamer plugins are installed type the following commands:

$ gst-inspect-1.0 | grep h264

To return all the H.264 related plugins, or:

$ gst-inspect-1.0 decodebin

To check directly the command.

To connect more than one board to the minicom, open it with the command:

$ sudo minicom –s

This way, you open the configuration menu. Enter in the “Serial port setup” option and press “A” to set or change the PORTNUMBER, in “ttyUSB$PORTNUMBER”.

To set the HDMI output, run the commands below from the U-Boot prompt:

=> setenv mmcargs 'setenv bootargs console=ttymxc0,115200 root=/dev/mmcblk2p2 rootwait rw video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24 consoleblank=0'

=> saveenv

Be sure that the IPs are correctly setted: SERVER:

=> ifconfig eth0 $SERVERIP

CLIENTS:

=> ifconfig eth0 $CLIENTSIP

Streaming transcoded video only

SERVER:

=> gst-launch-1.0 filesrc location=/home/root/bbb_720p.mp4 ! decodebin ! queue max-size-buffers=0 ! vpuenc_h264 gop-size=2 bitrate=20000 ! queue max-size-buffers=0 ! rtph264pay config-interval=2 ! queue max-size-buffers=0 ! gdppay ! tcpserversink blocksize=512000 host=$SERVERIP$ port=8554

CLIENTS:

=> gst-launch-1.0 tcpclientsrc host=$SERVERIP$ port=8554 ! gdpdepay ! queue max-size-buffers=0 ! 'application/x-rtp, media=(string)video, clock10-rate=(int)90000, payload=(int)96' ! queue max-size-buffers=0 ! rtpjitterbuffer latency=100 ! queue max-size-buffers=0 ! rtph264depay ! queue max-size-buffers=0 ! decodebin ! autovideosink sync=false

Streaming transcoded video + audio

SERVER:

=> gst-launch-1.0 filesrc location=/home/root/bbb_720p.mp4 ! decodebin name=demux demux. ! queue max-size-buffers=0 ! vpuenc_h264 gop-size=2 bitrate=20000 ! queue max-size-buffers=0 ! rtph264pay config-interval=2 ! queue max-size-buffers=0 ! gdppay ! tcpserversink blocksize=512000 host=$SERVERIP$ port=8554 demux. ! alsasink

CLIENTS:

=> gst-launch-1.0 tcpclientsrc host=$SERVERIP$ port=8554 ! gdpdepay ! queue max-size-buffers=0 ! 'application/x-rtp, media=(string)video, clock10-rate=(int)90000, encoding-name=(string)H264' ! queue max-size-buffers=0 ! rtpjitterbuffer latency=100 ! queue max-size-buffers=0 ! rtph264depay ! queue max-size-buffers=0 ! decodebin ! autovideosink sync=false

 

You can check the results with the 1080p@24fps.

无评分
版本历史
最后更新:
1 周之前
更新人: