Don't forget to update your source code.
How to customize the image
Enter <yocto>/source and find any image available:
$ find -name *image*.bb
./meta-fsl-demos/recipes-fsl/images/fsl-image-gui-sdk.bb
./meta-fsl-demos/recipes-fsl/images/fsl-image-test.bb
./meta-fsl-demos/recipes-fsl/images/fsl-image-gui.bb
./meta-fsl-demos/recipes-qt/images/qt-in-use-image.bb
./meta-fsl-demos/recipes-qt/images/qte-in-use-image.bb
./meta-openembedded/meta-initramfs/recipes-bsp/images/initramfs-kexecboot-klibc-image.bb
./meta-openembedded/meta-initramfs/recipes-bsp/images/initramfs-kexecboot-image.bb
./meta-openembedded/meta-oe/recipes-support/imagemagick/imagemagick_6.7.5.bb
./meta-openembedded/meta-oe/recipes-multimedia/libsdl-image/libsdl-image_1.2.12.bb
./poky/meta-hob/recipes-core/images/hob-image.bb
./poky/meta-skeleton/recipes-multilib/images/core-image-multilib-example.bb
./poky/meta/recipes-devtools/mkelfimage/mkelfimage_svn.bb
./poky/meta/recipes-sato/images/core-image-sato-dev.bb
./poky/meta/recipes-sato/images/core-image-sato.bb
./poky/meta/recipes-sato/images/core-image-sato-sdk.bb
./poky/meta/recipes-qt/images/qt4e-demo-image.bb
./poky/meta/recipes-core/images/core-image-minimal.bb
./poky/meta/recipes-core/images/core-image-base.bb
./poky/meta/recipes-core/images/core-image-minimal-dev.bb
./poky/meta/recipes-core/images/core-image-minimal-initramfs.bb
./poky/meta/recipes-core/images/build-appliance-image.bb
./poky/meta/recipes-core/images/core-image-minimal-mtdutils.bb
./poky/meta/recipes-extended/images/core-image-lsb-sdk.bb
./poky/meta/recipes-extended/images/core-image-basic.bb
./poky/meta/recipes-extended/images/core-image-lsb-dev.bb
./poky/meta/recipes-extended/images/core-image-lsb.bb
./poky/meta/recipes-graphics/images/core-image-directfb.bb
./poky/meta/recipes-graphics/images/core-image-x11.bb
./poky/meta/recipes-graphics/images/core-image-clutter.bb
./poky/meta/recipes-graphics/xcb/xcb-util-image_0.3.9.bb
./poky/meta/recipes-bsp/u-boot/u-boot-mkimage_2012.04.01.bb
./poky/meta/recipes-bsp/u-boot/u-boot-mkimage_2011.06.bb
./poky/meta/recipes-bsp/u-boot/u-boot-mkimage_2011.03.bb
./poky/meta/recipes-rt/images/core-image-rt-sdk.bb
./poky/meta/recipes-rt/images/core-image-rt.bb
The above images (and packages with 'image' in file name) may be used as a base image, where new packages may be added, or example of new images.
bitbake -s shows any *available* package locally. Grep for the name of desired package:
$ bitbake -s | grep calibrat
calibrateproto :0.0+gitAUTOINC+1da6fd1e2c7a49648245c98481fabea8b9690a8c-r2
libxcalibrate :0.0+gitAUTOINC+209d83af61ed38a002c8096377deac292b3e396c-r0
xinput-calibrator :0.7.5+gitAUTOINC+c01c5af807cb4b0157b882ab07a893df9a810111-r1
For example, the package name is xinput-calibrator, in order to include this package this would be the string needed.
The dependency tree is shown with
$ bitbake -g fsl-image-test
For the fsl-image-test. Or any other image
Include the package name on the image definition file.
$ cd meta-fsl-demos/
$ vim recipes-fsl/images/fsl-image-test.bb
Include the package name on IMAGE_INSTALL list:
IMAGE_INSTALL += " \
packagegroup-fsl-gstreamer \
packagegroup-fsl-tools-testapps \
packagegroup-fsl-tools-benchmark \
xinput-calibrator \
"
In order to include the package on any image, configure conf/local.conf file the as the following:
MACHINE ??= 'imx6qsabresd'
DISTRO ?= 'poky'
PACKAGE_CLASSES ?= "package_rpm"
EXTRA_IMAGE_FEATURES = "debug-tweaks tools-sdk"
USER_CLASSES ?= "buildstats image-mklibs image-prelink"
PATCHRESOLVE = "noop"
CONF_VERSION = "1"
BB_NUMBER_THREADS = '8'
PARALLEL_MAKE = '-j 8'
ACCEPT_FSL_EULA = "1"
CORE_IMAGE_EXTRA_INSTALL += "xinput-calibrator"
And then
$ bitbake fsl-image-test
In order to add debug or native builder include on conf/local.conf:
EXTRA_IMAGE_FEATURES += "tools-sdk"
Every image created after that will include development tools. The same may be included in any bb image file.
From Poky description:
'tools-sdk" - Adds development tools such as gcc, make, pkgconfig and so forth.
"dev-pkg" - Adds -dev packages for all installed packages. This is useful if you want to develop against the libraries in the image.
"tools-debug" - Adds debugging tools such as gdb and strace.
If you don't like command line, or you prefer a window-like interface, you can take a look on HOB.
See hob documentation https://www.yoctoproject.org/documentation/hob-manual
See getting started video for hob Introducing Hob - YouTube
Go to Yocto Training - HOME
Go to Task #5 - Kernel