Lighting Control Philips Hue Light Through KW20(Zigbee Coordinator) with i.MX6Q

cancel
Showing results for 
Search instead for 
Did you mean: 

Lighting Control Philips Hue Light Through KW20(Zigbee Coordinator) with i.MX6Q

No ratings

Lighting Control Philips Hue Light Through KW20(Zigbee Coordinator) with i.MX6Q

Hi all,

Most of IoT customers request to enable/demo i.MX EVK with FSL Zigbee solution. In default i.MX Linux/Android BSP, Zigbee function is not enabled. Here we make a lighting demo setup through i.MX6Q SabreSD, KW20 USB dongle and Philips Hue light. KW20 is configured as Zigbee coordinator, connected with USB OTG in i.MX6Q, then i.MX6Q can issue On/Off, brightness and color control commands through KW20 to toggle Philips Hue light directly.

Please find the attachment for details.

Best regards,

Carl

Attachments
Comments

Good share!!

This is very helpful.

Thanks a lot!!

Thanks for your share!

Hello! 

I tried to follow this guide but gets stuck on when to use Test Tool to send commands, I can't find the ZTC_ZllTouchLink...  commands. Are there something missing in my ZigBeePro.xml file, or what do I need to do?

Best Regards,

Mattias

Hello,

    ZTC_ZllTouchLink is not supported at existing released xml file. You may contact your local sales/FAE to get the xml version which support ZTC_ZllTouchLink command sets.    

Version history
Revision #:
1 of 1
Last update:
‎10-09-2014 12:25 AM
Updated by: