How to install Segger Firmware in MCU LINK PRO

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to install Segger Firmware in MCU LINK PRO

How to install Segger Firmware in MCU LINK PRO

What we need? 

  • USB cable
  • Windows Host PC
  • MCU-LINK PRO


What Do You Gain?

With this firmware upgrade, you will be able to debug the M core of i.MX processors (such as i.MX8 and i.MX9).

Also, the cost advantage due to the MCU-LINK PRO is currently the most affordable debugger available for i.MX processors.

 

Firmware Upgrade Steps

 

Install Required Tools

Install the MCUXpresso IDE, or use the MCUXpresso Installer for VS Code to install the necessary software tools.

Chavira_0-1747762120431.png

 

Chavira_1-1747762220719.png

 

Download Firmware

Get the latest firmware from the Segger web page

 

Save Firmware

Save the downloaded firmware in the following directory:

C:\nxp\LinkServer_1.6.133\MCU-LINK_installer\probe_firmware

 

Backup Old Firmware

Rename the existing firmware file to keep a backup.

 

Example:

Rename firmware.s19 to old_firmware.s19


Chavira_0-1747763129172.png

 

Set Jumper and Connect

Place a jumper on J4 and connect the MCU-LINK PRO to the host PC via USB.


Chavira_1-1747763160702.png

 

Open LinkServer CLI

Launch the LinkServer CLI.

If it's not installed, download it from NXP web page.

Chavira_2-1747762424078.png

 

Run the Update Script

Execute the following commands in the terminal:

$ cd MCU-LINK_installer
$ scripts\program_JLINK.cmd

 

Start Firmware Flash

Once the MCU-LINK PRO is detected, press any key to flash the Segger firmware.

 

Chavira_2-1747763399333.png

 

Finalize Update

After a successful update, remove the jumper from J4, disconnect and reconnect the MCU-LINK PRO

 

Verify Installation

You can confirm that the debug probe is recognized using MCUXpresso IDE, or MCUXpresso for VS Code


Chavira_0-1747764271147.pngChavira_1-1747764385447.png

 

 

References:

MCU-Link installation 

 

100% 有帮助 (1/1)
版本历史
最后更新:
‎05-30-2025 09:49 AM
更新人: