The Contiguous Memory Allocator (CMA) is a framework, which allows setting up a machine-specific configuration for physically-contiguous memory management. Memory for devices is then allocated according to that configuration. The main role of the framework is not to allocate memory, but to parse and manage memory configurations, as well as to act as an in-between between device drivers and pluggable allocators. It is thus not tied to any memory allocation method or strategy.
Various devices on embedded systems have no scatter-getter and/or IO map support and as such require contiguous blocks of memory to operate. They include devices such as cameras, hardware video decoders and encoders, etc. Such devices often require big memory buffers (a full HD frame is, for instance, more then 2 mega pixels large, i.e. more than 6 MB of memory), which makes mechanisms such as kmalloc() ineffective. Some embedded devices impose additional requirements on the buffers, e.g. they can operate only on buffers allocated in particular location/memory bank (if system has more than one memory bank) or buffers aligned to a particular memory boundary. Development of embedded devices have seen a big rise recently (especially in the V4L area) and many such drivers include their own memory allocation code. Most of them use bootmem-based methods. CMA framework is an attempt to unify contiguous memory allocation mechanisms and provide a simple API for device drivers, while staying as customisable and modular as possible.
Most of the i.MX SoC does not have IOMMU for specific IP who requires larger contiguous memory for operations, like VPU/GPU/ISI/CSI. Or they have IOMMU, but performance is not that good. In the default i.MX BSP, we still allocate physical contiguous memory for those IP drivers for DMA transfers.
In arm64 kernel, the DMA allocation API would allocate memory in a various way which depends on the device configurations (in dts or gfp flags). The below table shows how the DMA allocation API (w/o IOMMU enabled device) works to find a proper way for pages (by order, coherent pool -> CMA -> Buddy -> SWIOTLB):
Allocator (by order) | Configurations (w/o IOMMU) | Comments | Mapping |
---|---|---|---|
Coherent Pool |
|
By __alloc_from_pool() | Already mapped on boot when coherent pool init in VMALLOC |
CMA |
|
By cma_alloc() | map_vm_area, mapped in VMALLOC |
Buddy |
|
By __get_free_pages(), which can only allocate from the DMA/normal zone (lowmem), 32bits address spaces | Already mapped in the lowmem area by kernel on boot |
SWIOTLB |
|
By map_single() | Already mapped on boot when SWIOTLB init |
Also a diagram shows how it works (DMA allocation path):
By default, kernel uses CMA as a backend of DMA buffers allocation for most of the cases. That's why i.MX BSP use CMA in the default release for GPU/VPU/CSI/ISI or other buffers for DMA transfers.
Read cons statement above. The key point is to reserve memory for critical path of allocation like GPU graphic buffers and camera/VPU preview/recording buffers to keep a good user experience from allocation failure which would cause black screen, preview stuck, etc. Also avoid potential dead lock when CMA and FUSE work together.
To get rid of CMA, the basic idea is to cut off the CMA way in the DMA allocation, turn to coherent pool (atomic pool). Please not that coherent pool can only be used by DMA allocation API, it's not shared to system buddy.
Add “coherent_pool=<size>” in command line, Coherent pool is actually allocate from system default CMA, so CMA size > coherent_pool.
There's no reference for this size, as it's various from system to system and use cases to use cases:
The size must be verified by test to make sure system stable.
Hack to arch/arm64/mm/dma-mapping.c, remove the gfpflags_allow_blocking check in the __dma_alloc() function:
diff --git a/arch/arm64/mm/dma-mapping.c b/arch/arm64/mm/dma-mapping.c
index 7015d3e..ef30b46 100644
--- a/arch/arm64/mm/dma-mapping.c
+++ b/arch/arm64/mm/dma-mapping.c
@@ -147,7 +147,7 @@ static void *__dma_alloc(struct device *dev, size_t size,size = PAGE_ALIGN(size);
- if (!coherent && !gfpflags_allow_blocking(flags)) {
+ if (!coherent) { // && !gfpflags_allow_blocking(flags)) {
struct page *page = NULL;
void *addr = __alloc_from_pool(size, &page, flags);
In both Android and Yocto release, ION allocator (android staging driver) is used for VPU buffers. And it default goes into the ION CMA heap. This means ION request for contiguous memory is direct to CMA. To avoid CMA, we can use carveout heap instead of CMA heap in ION:
Enable CARVEOUT heap, disable CMA heap:
CONFIG_ION=y
CONFIG_ION_SYSTEM_HEAP=y
-CONFIG_ION_CMA_HEAP=y
+CONFIG_ION_CARVEOUT_HEAP=y
+CONFIG_ION_CMA_HEAP=n
Adjust the carveout reserved heap base address and size in the dts:
/ {
reserved-memory {
#address-cells = <2>;
#size-cells = <2>;
ranges;
carveout_region: imx_ion@0 {
compatible = "imx-ion-pool";
reg = <0x0 0xf8000000 0 0x8000000>;
};
};
};
yocto/build-8qm/tmp/work/aarch64-mx8-poky-linux/gstreamer1.0-plugins-base/1.14.4.imx-r0/git:
diff --git a/gst-libs/gst/allocators/gstionmemory.c b/gst-libs/gst/allocators/gstionmemory.c
index 1218c4a..12e403d 100644
--- a/gst-libs/gst/allocators/gstionmemory.c
+++ b/gst-libs/gst/allocators/gstionmemory.c
@@ -227,7 +227,8 @@ gst_ion_alloc_alloc (GstAllocator * allocator, gsize size,
}for (gint i=0; i<heapCnt; i++) {
- if (ihd[i].type == ION_HEAP_TYPE_DMA) {
+ if (ihd[i].type == ION_HEAP_TYPE_DMA ||
+ ihd[i].type == ION_HEAP_TYPE_CARVEOUT) {
heap_mask |= 1 << ihd[i].heap_id;
}
}
Hello @xinyu_chen,
I cannot find ion_carveout_heap.c file in recent Linux BSP.
Do you have any recommendation for LF5.x.x BSP version?
One quick way is bringing carvout allocator back by revert this commit:
commit eadbf7a34e44e8fb2e63142b992bf264ffb72bf9
Author: Nishka Dasgupta <nishkadg.linux@gmail.com>
Date: Wed Jul 3 13:48:41 2019 +0530staging: android: ion: Remove file ion_carveout_heap.c
Remove file ion_carveout_heap.c as its functions and definitions are not
used anywhere.
Issue found with Coccinelle.Signed-off-by: Nishka Dasgupta <nishkadg.linux@gmail.com>
Acked-by: Laura Abbott <labbott@redhat.com>
Link: https://lore.kernel.org/r/20190703081842.22872-1-nishkadg.linux@gmail.com
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>