How to emulate i.MX8QM 1.3GHz parts on i.MX8QM MEK with 1.6GHz part

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to emulate i.MX8QM 1.3GHz parts on i.MX8QM MEK with 1.6GHz part

How to emulate i.MX8QM 1.3GHz parts on i.MX8QM MEK with 1.6GHz part

Overview

 

This document intends to provide one reference how to emulate i.MX8QM 1.3GHz part running on i.MX8QM MEK with 1.6GHz part based on i.MX Linux BSP release.

 

You can find i.MX8QM/QP processors datasheet on NXP web:


 

Key differences between 1.3GHz part and 1.6GHz part is as follows:

Key Differences

1.6GHz part

1.3GHz part

8QM/8QP A72 core max frequency

1600MHz

1296MHz

8QM GPU max frequency

core 800MHz  shader 1000MHz

core 650MHz shader 700MHz

8QM VDD_GPU mode

Overdrive mode

Remove overdrive mode, only nominal

8QM VDD_GPU nominal operation range

Min 0.95V Typ 1.0 V Max 1.1V

Min 0.98V Typ 1.03125V Max 1.14V

 

Software Changes

 

Since Linux 6.6.23_2.0.0 BSP release, i.MX8QM/8QP 1.3GHz part is supported into i.MX Linux release by identifying the fuse of 1.3GHz part and configuring frequency and voltage automatically.

If you have i.MX8QM MEK board with 1.6GHz part, before revision E, you can apply software changes to emulate 1.3GHz part configurations explicitly.

The following software reference patches are built based on Linux 6.6.52-2.2.0 release:

Component

Patch Name

Description

Linux Kernel

0001-arm64-dts-imx8qm-remove-A72-core-1.6GHz-operating-po.patch

Used to remove Cortex-A72 core 1.6GHz operating-points

0002-arm64-dts-imx8qm-set-GPU-operating-points-at-nominal.patch

Used to remove GPU overdrive operating-points and set GPU core frequency as 650MHz, GPU shader frequency as 700MHz.

SCFW

0001-Increase-VDD-of-GPU.patch

Used to increase GPU voltage

ATF

0001-plat-imx8-make-ATF-kick-off-A72-core-freq-at-1.3GHz.patch

Used to kickoff A72 core and set its frequency as 1.3GHz in ATF

 

Validation Test

Apply patch into Linux kernel, SCFW porting kit, ATF, follow 6.6.52_2.2.0 release document(www.nxp.com/design/design-center/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-ap...) to build and deploy image.  

 

After Linux OS boot up,  run below command to check A72 and GPU frequency,  for example:

#cat /sys/kernel/debug/gc/clk

gpu0 mc clock: 647981058 HZ.

gpu0 sh clock: 695997687 HZ.

gpu1 mc clock: 647990370 HZ.

gpu1 sh clock: 695987994 HZ

 

#cat /sys/devices/system/cpu/cpu4/cpufreq/cpuinfo_max_freq

1296000

 

Measure VDD_GPU voltage from i.MX8QM MEK board TP53 and TP42

Untitled.png

附件
无评分
版本历史
最后更新:
‎04-08-2025 05:32 PM
更新人: