How to add 3G modem in Sabresx board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to add 3G modem in Sabresx board

How to add 3G modem in Sabresx board

Overview

The purpose of this document is to describe how to enable 3G modem in i.MX sabresx board for Android software.


Hardware Changes


Unlike other boards of I.mx series, in sabresx board  3G modem doesn't share to use PCIE slot any longer. It is not connected with PCIE slot by default. So if you still want to use 3G modem like in sabresd board. You need to do a tiny hardware rework. Like the below, R177 and R178 is DNP. Just add a zero resistor here.

Capture.PNG.png


Software patches

After you have do hardware rework above, then you should git am the attached patch to add software support which will add the dts config of 3G power. In our official release version, we don't include this patch.

ラベル(2)
添付
コメント

Hi waterzhou

I am working on i.MX 6 SoloX SABRE SD board to support a customer for 3G USB dongle for data connection.

The changes that you mentioned above are related to the PCIe interface.

Will the above changes also support/ applicable to  3G USB dongle?

How do we interface the 3G USB dongle with the PCIe Interface?

Thanks and Regards,

-Devaraj

評価なし
バージョン履歴
最終更新日:
‎06-30-2014 02:05 AM
更新者: